Cancel
Showing results for 
Search instead for 
Did you mean: 

Defining contact for Sol 701

Valued Contributor
Valued Contributor

Hello,

 

I have to model an impact on a bundle of tubes. Therefore it is necessary to define contact between all neighoring tubes and selfcontact inside each tube.

Is there any function available in Sol 701 which is similar to the General Contact option of Abaqus?

 

Using the automatic funciton is quite a lot of work, becaus it is also necessary to consider that each tube needs to be considered as source and target.

 

Thanks for your comments.

 

Bundle of tubes.png

3 REPLIES

Re: Defining contact for Sol 701

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

In the animated SOL701 model below only TWO REGIONS exist:

  • Region#1 (SOURCE): all the exterior faces of all blocks.
  • Region#2 (TARGET): the faces of the wall external frame.

And only TWO CONNECTOR exist:

  • SELF-CONTACT: Region#1 with Region#1.
  • BLOCKS-WALL: Region#1 with Region#2

 

 

Then at the beginning it seems very complex, but sometimes defining contact is very simply and straightforward, give it a try!.

 

Here you have more examples of NX NASTRAN Advanced Nonlinear Module:

http://iberisa.wordpress.com/2011/12/05/analisis-no-lineal-avanzado-con-femap-y-nx-nastran-sol601701...

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Defining contact for Sol 701

Valued Contributor
Valued Contributor

Hello Blas!

 

Thank you for your answer and for the link. I guess I will also try some of this examples to get more experienced with NX Advanced Nonlinear.

 

Best regards,

 

Georg

Re: Defining contact for Sol 701

Siemens Genius Siemens Genius
Siemens Genius

Also, remember to take advantage of symmetry. This will reduce your problem size.