Cancel
Showing results for 
Search instead for 
Did you mean: 

Deflected mesh from nastran result file into NX

N/A

Hi There,
Is it possible in NX6.0 UGI to have a deflected mesh from a displacement plot in
OP2 file?
Engrequest,
Many thanks
3 REPLIES

Re: Deflected mesh from nastran result file into NX

Siemens Builder Siemens Builder
Siemens Builder
You will be able to do this in NX 7.5 directly using fields.

In NX 7.0, two NX Open routines were delivered in the UGII_BASE_DIR\UGOPEN\SampleNXOpenApplications\.NET\CAE that will do this. They should run in NX 6.x as well.


DeformMeshFromSolutionResults


    This will update the node coordinates using displacement results data from the current solution

DeformMeshFromResultFile


    This will prompt the user to select a solver output file, then deform the mesh based on the selected displacement results.

--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm

Re: Deflected mesh from nastran result file into NX

N/A

Thanks tsbernar! But do i need to create a CAE folder (i am using NX6.0) and stick
the routines into it?
how does it work then from UGInterface?
Engrequest,
many thanks

tsbernar wrote:
>
>You will be able to do this in NX 7.5 directly using fields.
>
>In NX 7.0, two NX Open routines were delivered in the
>UGII_BASE_DIR\UGOPEN\SampleNXOpenApplications\.NET\CAE that will do
>this. They should run in NX 6.x as well.
>
>
>- DeformMeshFromSolutionResults
>
>
> - This will update the node coordinates using displacement results
> data from the current solution
>
>- DeformMeshFromResultFile
>
>
> - This will prompt the user to select a solver output file, then
> deform the mesh based on the selected displacement
> results.
>
>
>+-------------------------------------------------------------------+
>|Filename: DeformMeshNX7.zip |
>|Download: http://bbsnotes.ugs.com/vbulletin/attachment.php?attachmentid=410|
>+-------------------------------------------------------------------+
>
>--
>tsbernar
>------------------------------------------------------------------------
>tsbernar's Profile: http://bbsnotes.ugs.com/vbulletin/member.php?userid=191178
>View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=40465
>

Re: Deflected mesh from nastran result file into NX

Siemens Builder Siemens Builder
Siemens Builder
Download the file and extract the contents. Each folder contains a readme text file that describes how to use the utility.
--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm