Cancel
Showing results for 
Search instead for 
Did you mean: 

Direct Transient Analysis in NX

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

I’m interested in direct transient analysis in NX (SOL 109). I can do this kind of analysis in FEMAP while there is tutorial of example. The point of this simulation should be load as a function of time. I don’t know how to set this time dependent load.

Can anybody provide some short guideline or model?

Juraj

1 REPLY

Re: Direct Transient Analysis in NX

Creator
Creator

Hi,

In NX, you must create a table in order to define a time dependent load :

- In Load Type, choose Force for example.

- In the Magnitude field, click the = symbol, then New Field, then Table....

- In Independent list, choose Time.

- Now enter the different Data Points you need to define, with the syntax time, force. There's also the possibility to read from a text file or a Excel file.

  Christophe