Cancel
Showing results for 
Search instead for 
Did you mean: 

Distance between two nodes

Pioneer
Pioneer
Hello expert,

i was trying to measure the distance between two nodes on imported mesh, where i don't have geometry, but i couldn't measure, can you please tell me the procedure to measure the distance in the absence of geometry.

Can we crate a point at a node if yes how?

Thank you.
1 REPLY

Re: Distance between two nodes

Siemens Builder Siemens Builder
Siemens Builder
You should be able to pick nodes directly in the measure command. Check the following:

1) Nodes are visible. Use show/hide to toggle all entities off then on
2) No selection filter is set when you are in the measure command
3) Selection scope is set to "Entire Assembly"
4) Snap Points are enabled in the Selection bar and "Existing Point" is toggled on

Regards,
--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm