Showing results for 
Search instead for 
Do you mean 
Reply

ERROR WITH SOL 601


Hi all,
iam performing an advanced non Linear analysis, and the solve crashes after starting
with the error:
*** MEMORY REALLOCATION ***
REQUESTED MEMORY FROM THE SYSTEM...= 2192.0 mb ( 274.0 mw)
Re-allocating 2194.4 MB of memory ...

ELEMENT GROUP = 53 (SHELL ELEMENT / SHELTH)
ELEMENT NUMBER= 744237
NPAR(6) = 0
SINCE NODES OF THIS ELEMENT REFER TO SKEW COORDINATE
SYSTEM(S), NPAR(6) MUST BE SET TO 1.
S T O P
*** ERROR NO. A1397 ***
Error in the element group control parameters,skew systems not indicated
PROGRAM SOL601, build date: 09.12.2008 *** NO HEADING DEFINED ***
Do you have any idea what is this related to?
Many Thanks,
1 REPLY

Re: ERROR WITH SOL 601

I've not seen this error before. It appears to be in Adina format and is referring to an element that references nodes that are defined in a local (skew) coordinate system.

I'm not sure what NX Nastan parameter maps to the Adina NPAR(6) parameter. Please contact GTAC and submit a PR so that we can determine the cause and get the error trapped with NX Nastran messaging in a future release.

Regards,
Jim
--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm