Cancel
Showing results for 
Search instead for 
Did you mean: 

Error during opening SIM- und FEM-File

Creator
Creator

Hello,

 

when opening a .sim file, the attached error message appears.

According to the error message, NX 10 has problems reading the associated .fem file of the .sim file. As I tries to load just the .fem-file, the same error message appears and the loading process terminates at 45%.

The .fem file was created with the same Siemens NX (same license and version). The memory of 128 GB is hardly used during the loading process.

The .fem file has a size of 3,054 GB and is stored in the following folder: "D: \ Pfaller \ SIMV \ SIMV_2" (in terms of path length).

Please let me know how I can fix the error as it already appears with other models. Thank you very much.

Best regards

 

Werner

1 REPLY

Re: Error during opening SIM- und FEM-File

Creator
Creator

Hi,

 

is there a limitation of the .FEM-file size?

 

When I try to open a .FEM-file with a size of 1.5 GB it works perfectly fine - a file with a size of 2.5 GB has problems.

 

Thanks for your support.

 

Best regards

 

Werner