Showing results for 
Search instead for 
Do you mean 
Reply

Error installing NX Nastran 6.1 on Linux openSUSE 11


Hello!,
Installing NX Nastran in Linux openSUSE as SuperUserI get the following error:
# ./nxnsetup
NXNSETUP January 26, 2009
ERROR: Could not find "/usr/bin/rsh".
alias rsh="/usr/bin/rsh"

What means this error?. Thanks for help.
Best regards,
Blas.
1 REPLY

Re: Error installing NX Nastran 6.1 on Linux openSUSE 11


Blas Molero wrote:
> Hello!,
> Installing NX Nastran in Linux openSUSE as SuperUserI get the following error:
>
> # ./nxnsetup
> NXNSETUP January 26, 2009
>
> ERROR: Could not find "/usr/bin/rsh".
> alias rsh="/usr/bin/rsh"
>
>
>
> What means this error?. Thanks for help.
> Best regards,
> Blas.

It seams rsh is not installed in your linux distro or rsh is not found
in your path.
You can try two things:
1) Easy one. How did you get superuser privilegies? If you have run "su"
command from an ordinary user try "su -" command (with a slash (-) after
su) then the environment variables belong to root user and perhaps rsh
will be in the path. Then try again ./nxnsetup
2) Hardest one. rsh in not installed so, you need to install it.
Try to install rsh and in the license server (I suppose is the same
machine) I think you will need to install also the rshd (rsh server
daemon).
I have never installed NX Nastran in linux, but technically speaking the
remote shell (rsh) needs a remote server daemon (rshd) in order to
work properly. This rshd is running through inet server daemon.
Hope this helps.
Frank.