Cancel
Showing results for 
Search instead for 
Did you mean: 

Error outputing the Result File

N/A

Hi
We are getting an Error " Nastran Executable not found " ( see Attachment ) when
we want to outpunt the Result file. The Whole setting up work fine ( Strenght Wizzard
O.K. ) but at the end this error come up ( NX4 )
Can anybody help.
Thank you
Roland
1 REPLY

Re: Error outputing the Result File

N/A

"Roland Hofmann" wrote:
>
>
>
>Hi
>
>We are getting an Error " Nastran Executable not found " ( see Attachment
>) when
>we want to outpunt the Result file. The Whole setting up work fine ( Strenght
>Wizzard
>O.K. ) but at the end this error come up ( NX4 )
>
>Can anybody help.
>
>Thank you
>
>Roland

Roland,
The Strength Wizard is setup to use NX Nastran as the solver.
- In NX4, NX Nastran must be installed in a separate install process from a separate
CD than NX. Did your sys admin install NX Nastran?
- Assuming NX Nastran is installed, UGII_NX_NASTRAN must be defined to point to
the bin directory in the NX Nastran installation. This can be defined in ugii_env.dat
in the NX UGII folder, or as a system environmental variable.
The error message you are getting is stating that UGII_NX_NASTRAN is set to C:\Program
Files\UG_NX4\UGSTRUCTURES and that nastran.exe is not at that location.
When you do install NX Nastran, do NOT install it in a folder with a pathname that
contains a space (or any special characters). I.e. do NOT install to C:\Program
Files\NX_Nastran\...
Jim