Cancel
Showing results for 
Search instead for 
Did you mean: 

FATAL error in SOL112 run

Experimenter
Experimenter

Hi All,

I am getting the following error in Modal Transient run(Refer the below f06 file). FE model is perfect it is solved without any error in modal & static check runs. In this problem applied loads are 246, I thought there could be problem with Residual vector calculations with NX-NASTRAN. When I solved without residual vectors(PARAM,RESVEC,NO), It is solved without any errors.But It is better to include residual vectors in the SOL112 to improve the accuracy of solution.

Please reply me if you have any suggestion. Thanks in advance

 

########################################abridged f06 ###########################

                          E I G E N V A L U E  A N A L Y S I S   S U M M A R Y   (READ MODULE)

 

                                     BLOCK SIZE USED ......................    7

                                     NUMBER OF DECOMPOSITIONS .............    2

                                     NUMBER OF ROOTS FOUND ................   79

                                     NUMBER OF SOLVES REQUIRED ............   30

1                                                                          NOVEMBER   1, 2017  NX NASTRAN 10/10/14   PAGE 44266
                                                                                                                                   
0                                                                                                                                  
 
                                              R E A L   E I G E N V A L U E S
                                         (BEFORE AUGMENTATION OF RESIDUAL VECTORS)
   MODE    EXTRACTION      EIGENVALUE            RADIANS             CYCLES            GENERALIZED         GENERALIZED
    NO.       ORDER                                                                       MASS              STIFFNESS
        1         1        1.402971E+00        1.184471E+00        1.885144E-01        1.000000E+00        1.402971E+00
        2         2        1.502212E+00        1.225647E+00        1.950678E-01        1.000000E+00        1.502212E+00
        3         3        2.113125E+00        1.453659E+00        2.313570E-01        1.000000E+00        2.113125E+00
        4         4        5.054173E+00        2.248149E+00        3.578040E-01        1.000000E+00        5.054173E+00
        5         5        1.425461E+01        3.775527E+00        6.008938E-01        1.000000E+00        1.425461E+01
        6         6        2.279118E+01        4.774011E+00        7.598073E-01        1.000000E+00        2.279118E+01
        7         7        1.002290E+03        3.165896E+01        5.038680E+00        1.000000E+00        1.002290E+03
        8         8        2.872389E+03        5.359468E+01        8.529858E+00        1.000000E+00        2.872389E+03
        9         9        3.588667E+03        5.990548E+01        9.534253E+00        1.000000E+00        3.588667E+03
       10        10        3.840051E+03        6.196815E+01        9.862536E+00        1.000000E+00        3.840051E+03
       11        11        5.588500E+03        7.475626E+01        1.189783E+01        1.000000E+00        5.588500E+03
       12        12        7.186529E+03        8.477340E+01        1.349211E+01        1.000000E+00        7.186529E+03
       13        13        8.481187E+03        9.209336E+01        1.465711E+01        1.000000E+00        8.481187E+03
       14        14        9.925640E+03        9.962750E+01        1.585621E+01        1.000000E+00        9.925640E+03
       15        15        1.354159E+04        1.163683E+02        1.852059E+01        1.000000E+00        1.354159E+04
       16        16        1.533024E+04        1.238153E+02        1.970582E+01        1.000000E+00        1.533024E+04
       17        17        1.681627E+04        1.296776E+02        2.063882E+01        1.000000E+00        1.681627E+04
       18        18        1.795560E+04        1.339985E+02        2.132653E+01        1.000000E+00        1.795560E+04
       19        19        1.931301E+04        1.389713E+02        2.211796E+01        1.000000E+00        1.931301E+04
       20        20        1.952312E+04        1.397252E+02        2.223795E+01        1.000000E+00        1.952312E+04
       21        21        2.086488E+04        1.444468E+02        2.298942E+01        1.000000E+00        2.086488E+04
       22        22        2.259992E+04        1.503327E+02        2.392619E+01        1.000000E+00        2.259992E+04
       23        23        2.386365E+04        1.544786E+02        2.458604E+01        1.000000E+00        2.386365E+04
       24        24        2.472380E+04        1.572380E+02        2.502521E+01        1.000000E+00        2.472380E+04
       25        25        2.623108E+04        1.619601E+02        2.577675E+01        1.000000E+00        2.623108E+04
       26        26        2.687461E+04        1.639348E+02        2.609103E+01        1.000000E+00        2.687461E+04
       27        27        2.770857E+04        1.664589E+02        2.649276E+01        1.000000E+00        2.770857E+04
       28        28        3.086735E+04        1.756911E+02        2.796210E+01        1.000000E+00        3.086735E+04
       29        29        3.192489E+04        1.786754E+02        2.843707E+01        1.000000E+00        3.192489E+04
       30        30        3.288229E+04        1.813347E+02        2.886032E+01        1.000000E+00        3.288229E+04
       31        31        3.371449E+04        1.836151E+02        2.922324E+01        1.000000E+00        3.371449E+04
       32        32        3.478254E+04        1.865008E+02        2.968252E+01        1.000000E+00        3.478254E+04
       33        33        3.781573E+04        1.944627E+02        3.094970E+01        1.000000E+00        3.781573E+04
       34        34        3.863021E+04        1.965457E+02        3.128122E+01        1.000000E+00        3.863021E+04
       35        35        3.917111E+04        1.979169E+02        3.149945E+01        1.000000E+00        3.917111E+04
       36        36        4.374612E+04        2.091557E+02        3.328817E+01        1.000000E+00        4.374612E+04
       37        37        4.426860E+04        2.104010E+02        3.348637E+01        1.000000E+00        4.426860E+04
       38        38        4.718302E+04        2.172165E+02        3.457108E+01        1.000000E+00        4.718302E+04
       39        39        4.759795E+04        2.181695E+02        3.472276E+01        1.000000E+00        4.759795E+04
       40        40        4.866586E+04        2.206034E+02        3.511012E+01        1.000000E+00        4.866586E+04
       41        41        4.973870E+04        2.230217E+02        3.549501E+01        1.000000E+00        4.973870E+04
       42        42        5.444259E+04        2.333294E+02        3.713552E+01        1.000000E+00        5.444259E+04
       43        43        5.753350E+04        2.398614E+02        3.817513E+01        1.000000E+00        5.753350E+04
       44        44        5.976063E+04        2.444599E+02        3.890699E+01        1.000000E+00        5.976063E+04
       45        45        6.040224E+04        2.457687E+02        3.911530E+01        1.000000E+00        6.040224E+04
       46        46        6.340224E+04        2.517980E+02        4.007490E+01        1.000000E+00        6.340224E+04
       47        47        6.900587E+04        2.626897E+02        4.180836E+01        1.000000E+00        6.900587E+04
       48        48        6.974405E+04        2.640910E+02        4.203139E+01        1.000000E+00        6.974405E+04
       49        49        7.284675E+04        2.699014E+02        4.295613E+01        1.000000E+00        7.284675E+04
       50        50        7.540597E+04        2.746015E+02        4.370418E+01        1.000000E+00        7.540597E+04
1                                                                          NOVEMBER   1, 2017  NX NASTRAN 10/10/14   PAGE 44267
                                                                                                                                   
0                                                                                                                                  
 
                                              R E A L   E I G E N V A L U E S
                                         (BEFORE AUGMENTATION OF RESIDUAL VECTORS)
   MODE    EXTRACTION      EIGENVALUE            RADIANS             CYCLES            GENERALIZED         GENERALIZED
    NO.       ORDER                                                                       MASS              STIFFNESS
       51        51        7.622495E+04        2.760887E+02        4.394088E+01        1.000000E+00        7.622495E+04
       52        52        7.989625E+04        2.826592E+02        4.498661E+01        1.000000E+00        7.989625E+04
       53        53        8.181339E+04        2.860304E+02        4.552315E+01        1.000000E+00        8.181339E+04
       54        54        8.447987E+04        2.906542E+02        4.625905E+01        1.000000E+00        8.447987E+04
       55        55        8.600484E+04        2.932658E+02        4.667471E+01        1.000000E+00        8.600484E+04
       56        56        8.826224E+04        2.970896E+02        4.728328E+01        1.000000E+00        8.826224E+04
       57        57        8.973193E+04        2.995529E+02        4.767532E+01        1.000000E+00        8.973193E+04
       58        58        9.182864E+04        3.030324E+02        4.822910E+01        1.000000E+00        9.182864E+04
       59        59        9.603815E+04        3.099002E+02        4.932215E+01        1.000000E+00        9.603815E+04
       60        60        9.807240E+04        3.131651E+02        4.984178E+01        1.000000E+00        9.807240E+04
       61        61        1.023781E+05        3.199658E+02        5.092413E+01        1.000000E+00        1.023781E+05
       62        62        1.030162E+05        3.209615E+02        5.108260E+01        1.000000E+00        1.030162E+05
       63        63        1.061478E+05        3.258033E+02        5.185321E+01        1.000000E+00        1.061478E+05
       64        64        1.068877E+05        3.269369E+02        5.203362E+01        1.000000E+00        1.068877E+05
       65        65        1.080651E+05        3.287325E+02        5.231940E+01        1.000000E+00        1.080651E+05
       66        66        1.133946E+05        3.367412E+02        5.359402E+01        1.000000E+00        1.133946E+05
       67        67        1.138031E+05        3.373472E+02        5.369047E+01        1.000000E+00        1.138031E+05
       68        68        1.147379E+05        3.387299E+02        5.391053E+01        1.000000E+00        1.147379E+05
       69        69        1.167195E+05        3.416423E+02        5.437407E+01        1.000000E+00        1.167195E+05
       70        70        1.212378E+05        3.481922E+02        5.541651E+01        1.000000E+00        1.212378E+05
       71        71        1.220438E+05        3.493477E+02        5.560041E+01        1.000000E+00        1.220438E+05
       72        72        1.234258E+05        3.513201E+02        5.591433E+01        1.000000E+00        1.234258E+05
       73        73        1.244743E+05        3.528092E+02        5.615133E+01        1.000000E+00        1.244743E+05
       74        74        1.258839E+05        3.548012E+02        5.646836E+01        1.000000E+00        1.258839E+05
       75        75        1.281095E+05        3.579239E+02        5.696535E+01        1.000000E+00        1.281095E+05
       76        76        1.303102E+05        3.609851E+02        5.745256E+01        1.000000E+00        1.303102E+05
       77        77        1.342560E+05        3.664096E+02        5.831590E+01        1.000000E+00        1.342560E+05
       78        78        1.360883E+05        3.689015E+02        5.871249E+01        1.000000E+00        1.360883E+05
       79        79        1.378636E+05        3.712999E+02        5.909422E+01        1.000000E+00        1.378636E+05
1                                                                          NOVEMBER   1, 2017  NX NASTRAN 10/10/14   PAGE 44268
                                                                                                                                   
0                                                                                                                                  
 ^^^ USER INFORMATION MESSAGE 9037 (RESVEC  )   
 ^^^ CHECKING RESIDUAL VECTORS FOR LINEAR INDEPENDENCE. 
 *** SYSTEM WARNING MESSAGE 6731 (SDCBOD)
    ROW  6199 OF LOWER TRIANGULAR FACTOR HAS DIAGONAL TERM = 0( OR .LT. 0 IF CHOLESKY )
 *** SYSTEM INFORMATION MESSAGE 4214 (SDCBOD)
      1.0E-10 SUBSTITUTED FOR DIAG. TERM OF LOWER TRIANGULAR FACTOR AT ROW   6199
 *** SYSTEM WARNING MESSAGE 6731 (SDCBOD)
    ROW  6202 OF LOWER TRIANGULAR FACTOR HAS DIAGONAL TERM = 0( OR .LT. 0 IF CHOLESKY )
 *** SYSTEM INFORMATION MESSAGE 4214 (SDCBOD)
      1.0E-10 SUBSTITUTED FOR DIAG. TERM OF LOWER TRIANGULAR FACTOR AT ROW   6202
 *** SYSTEM WARNING MESSAGE 6731 (SDCBOD)
    ROW  8645 OF LOWER TRIANGULAR FACTOR HAS DIAGONAL TERM = 0( OR .LT. 0 IF CHOLESKY )
 *** SYSTEM INFORMATION MESSAGE 4214 (SDCBOD)
      1.0E-10 SUBSTITUTED FOR DIAG. TERM OF LOWER TRIANGULAR FACTOR AT ROW   8645
 *** SYSTEM WARNING MESSAGE 6731 (SDCBOD)
    ROW  8947 OF LOWER TRIANGULAR FACTOR HAS DIAGONAL TERM = 0( OR .LT. 0 IF CHOLESKY )
 *** SYSTEM INFORMATION MESSAGE 4214 (SDCBOD)
      1.0E-10 SUBSTITUTED FOR DIAG. TERM OF LOWER TRIANGULAR FACTOR AT ROW   8947
 *** SYSTEM WARNING MESSAGE 6731 (SDCBOD)
    ROW  9635 OF LOWER TRIANGULAR FACTOR HAS DIAGONAL TERM = 0( OR .LT. 0 IF CHOLESKY )
 *** SYSTEM INFORMATION MESSAGE 4214 (SDCBOD)
      1.0E-10 SUBSTITUTED FOR DIAG. TERM OF LOWER TRIANGULAR FACTOR AT ROW   9635
 *** USER INFORMATION MESSAGE 4158 (SDCBOD)
     STATISTICS FOR SYMMETRIC DECOMPOSITION OF DATA BLOCK MZZ      FOLLOW
           MAXIMUM RATIO OF MATRIX DIAGONAL TO FACTOR DIAGONAL = 9.0E+15 AT ROW NUMBER   1352
 ^^^ THE FOLLOWING MODE SHAPES (EIGENVECTORS OR RESIDUAL VECTORS) ARE NOT LINEARLY INDEPENDENT WITH OTHER MODE                    
     SHAPES AND WILL BE DISCARDED.  
 ^^^ MZZ MATRIX DIAGONALS/FACTOR DIAGONALS,RESVRAT=   1.000000E+08
1                                                                          NOVEMBER   1, 2017  NX NASTRAN 10/10/14   PAGE 44269
                                                                                                                                   
0                                                                                                                                  
0                BIGRATS                                                                                                           
     POINT           VALUE     POINT           VALUE     POINT           VALUE     POINT           VALUE     POINT           VALUE 
                                                                                                                                   

 COLUMN           1
        358  H  1.28349E+08       418  H  1.41190E+08       561  H  2.00160E+14       562  H  2.45428E+13       563  H -3.54614E+13
        564  H  9.00720E+14       565  H -5.36143E+13       566  H -1.87650E+14       628  H  1.09345E+08       658  H  1.33669E+08
        703  H  1.57468E+08       820  H  1.15504E+08       823  H  2.03410E+08       825  H  2.72945E+14       826  H  2.19688E+14
        827  H -1.02355E+14       828  H  2.78861E+13       829  H -1.07229E+14       830  H -3.21686E+14       831  H  4.31173E+12
        832  H  2.81475E+14       833  H -4.09418E+13       834  H -1.95809E+14       835  H  3.46431E+14       836  H  3.00240E+15
        847  H  1.09370E+08       850  H  1.50434E+08       853  H  2.75348E+08       907  H  1.14706E+08       910  H  2.06344E+08
        931  H  1.74390E+08       934  H  1.25179E+08       937  H  2.16511E+08       939  H  7.50600E+14       940  H -8.49736E+13
        941  H -1.80144E+14       942  H -2.43438E+14       943  H -1.99274E+13       944  H  5.62950E+14      1198  H  1.40512E+08
       1315  H  1.03505E+08      1333  H  1.08083E+08      1342  H  1.30334E+08      1344  H -4.01928E+12      1345  H  1.63767E+14
       1346  H  4.07566E+13      1347  H -7.38295E+13      1348  H -1.73215E+14      1349  H -4.89522E+13      1350  H  1.54233E+13
       1351  H  7.03687E+13      1352  H  9.00720E+15      1353  H -7.50600E+14      1354  H -1.47417E+13      1355  H -4.09418E+14
       1356  H  7.20576E+13      1357  H  6.38808E+13      1358  H -1.24066E+13      1359  H  3.19404E+13      1360  H -3.75300E+14
       1361  H  7.01495E+12      1363  H  1.12301E+08      1402  H  1.62668E+08      1450  H  1.11939E+08      1453  H  1.41056E+08
       1456  H  2.40444E+08      1465  H  1.32087E+08      1468  H  2.35901E+08      1507  H  1.05246E+08      1510  H  1.17962E+08
       1513  H  1.38084E+08      1516  H  1.77590E+08      1519  H  3.08006E+08      1582  H  1.50780E+08      1612  H  1.34797E+08
       1657  H  1.55673E+08      1774  H  1.27558E+08      1777  H  2.23231E+08      1779  H -2.90555E+13      1780  H -2.14457E+14
       1781  H  3.78454E+13      1782  H  1.80867E+13      1783  H -8.18836E+13      1784  H -1.28674E+14      1792  H  1.01389E+08
       1795  H  1.26402E+08      1798  H  1.73933E+08      1801  H  3.18423E+08      1852  H  1.35543E+08      1855  H  2.43406E+08
       1867  H  1.11173E+08      1873  H  1.06112E+08      1876  H  2.06918E+08      2088  H  2.57349E+14      2089  H -7.14857E+13
       2090  H  6.60352E+12      2091  H  1.09178E+13      2092  H -3.49116E+13      2093  H -5.03195E+12      2094  H -5.62950E+14
       2095  H  8.34000E+13      2096  H -2.81475E+14      2097  H  4.52623E+13      2098  H -5.70076E+13      2099  H  2.55161E+13
       2100  H  1.73215E+14      2101  H  3.84923E+13      2102  H -2.05644E+13      2103  H -4.50360E+15      2104  H  2.81475E+14
       2105  H  1.15923E+13      2212  H  1.21133E+08      2377  H  1.04304E+08      2380  H  1.83815E+08      2428  H  1.12126E+08
       2431  H  1.97524E+08      2503  H  1.53674E+08      3478  H  1.03517E+08      3622  H  1.15365E+08      3718  H  1.05730E+08
       3870  H -1.17741E+13      3871  H  9.00720E+14      3872  H -1.23776E+12      3873  H  3.91617E+14      3874  H -1.04371E+13
       3875  H  7.56908E+13      3876  H -2.04709E+14      3877  H -1.23386E+14      3878  H  4.22873E+12      3879  H -1.28674E+15
       3880  H -5.00400E+13      3881  H  3.88074E+12      3882  H  1.18516E+14      3883  H -2.89714E+12      3884  H  1.83820E+14
       3885  H -6.77233E+13      3886  H  6.34310E+13      3887  H -4.84258E+13      3937  H  1.22893E+08      4078  H  1.03245E+08
       4087  H  1.28439E+08      4089  H -1.12590E+14      4090  H -1.21719E+14      4091  H  7.91494E+12      4092  H  1.49621E+13
       4093  H  2.40192E+13      4094  H -1.55297E+14      4095  H  2.75450E+13      4096  H  3.75300E+14      4097  H -7.60743E+12
       4098  H  1.77307E+13      4099  H -2.50200E+13      4100  H -2.64918E+14      4101  H  4.92197E+13      4102  H  1.02355E+14
       4103  H -1.93703E+13      4104  H -3.75300E+14      4105  H -6.43371E+13      4106  H  1.68359E+13      4108  H  1.11265E+08
       4174  H  1.29104E+08      4177  H  2.30506E+08      4213  H  1.60121E+08      4252  H  1.03249E+08      4255  H  1.15649E+08
       4258  H  1.35295E+08      4261  H  1.73907E+08      4264  H  3.01469E+08      4288  H  1.35671E+08      4360  H  1.33323E+08
       4420  H  1.55392E+08      4453  H  1.02373E+08      4456  H  1.81569E+08      4468  H  1.70917E+08      4543  H  1.37749E+08
       4735  H  1.63553E+08      4750  H  1.47952E+08      4822  H  1.39200E+08      4825  H  1.43638E+08      4828  H  2.48325E+08
       4830  H  1.47417E+13      4831  H -1.34436E+14      4832  H  1.37514E+13      4833  H -1.86484E+13      4834  H  5.81110E+13
       4835  H  1.51382E+13      4846  H  1.01106E+08      4849  H  1.76287E+08      4918  H  1.02286E+08      4921  H  1.78805E+08
       4923  H  1.36473E+14      4924  H -1.18050E+13      4925  H -3.38617E+13      4926  H  6.04510E+13      4927  H -1.32459E+13
       4928  H -6.10244E+12      4929  H -5.23674E+13      4930  H  4.46786E+12      4931  H -9.19102E+13      4932  H  1.40081E+13
       4933  H -7.16563E+12      4934  H -4.94629E+12      4935  H -4.02107E+13      4936  H  5.92579E+13      4937  H -1.52664E+13
       4938  H -3.60288E+14      4939  H  1.19713E+12      4940  H  1.18360E+13      4941  H -1.94961E+13      4942  H  1.60556E+13
       4943  H  1.13298E+13      4944  H -8.41794E+13      4945  H -2.25180E+14      4946  H  8.44161E+12      4947  H  2.86853E+13
       4948  H  1.21719E+14      4949  H -5.59453E+13      4950  H -2.37032E+14      4951  H -1.16977E+14      4952  H  4.86876E+13
       4953  H  3.50475E+13      4954  H -7.26387E+13      4955  H  4.85563E+12      4956  H -1.20096E+14      4957  H  5.11482E+12
       4958  H  1.60843E+14      4959  H -2.38918E+13      4960  H  4.24868E+13      4961  H -1.60556E+13      4962  H -7.44397E+13
       4963  H -1.12590E+15      4964  H  5.61931E+11      4965  H  8.18836E+14      4966  H -3.26348E+13      4967  H  2.29191E+13
       4968  H  1.60843E+14      4969  H -1.66800E+14      4970  H -2.81475E+14      4971  H -4.54909E+13      4972  H  3.31147E+13
1                                                                          NOVEMBER   1, 2017  NX NASTRAN 10/10/14   PAGE 44270
                                                                                                                                   
0                                                                                                                                   
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  9.869604D+34, CYCLES =  5.000000D+16 NUMBER OF EIGENVALUES BELOW THIS VALUE =  4737
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  1.378639D+05, CYCLES =  5.909427D+01 NUMBER OF EIGENVALUES BELOW THIS VALUE =    79
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  4.834454D+06, CYCLES =  3.499402D+02 NUMBER OF EIGENVALUES BELOW THIS VALUE =   162
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  1.565833D+07, CYCLES =  6.297858D+02 NUMBER OF EIGENVALUES BELOW THIS VALUE =   227
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  4.697499D+07, CYCLES =  1.090821D+03 NUMBER OF EIGENVALUES BELOW THIS VALUE =   300
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  1.409250D+08, CYCLES =  1.889357D+03 NUMBER OF EIGENVALUES BELOW THIS VALUE =   387
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  4.475564D+08, CYCLES =  3.367007D+03 NUMBER OF EIGENVALUES BELOW THIS VALUE =   509
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  1.342669D+09, CYCLES =  5.831827D+03 NUMBER OF EIGENVALUES BELOW THIS VALUE =   628
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  4.065769D+09, CYCLES =  1.014826D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =   783
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  1.219731D+10, CYCLES =  1.757730D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =   984
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  3.659192D+10, CYCLES =  3.044477D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =  1268
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  2.370574D+10, CYCLES =  2.450456D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =  1144
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  1.097758D+11, CYCLES =  5.273189D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =  1684
1                                                                          NOVEMBER   1, 2017  NX NASTRAN 10/10/14   PAGE 44290
                                                                                                                                   
0                                                                                                                                  
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  6.441048D+10, CYCLES =  4.039228D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =  1462
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  3.293273D+11, CYCLES =  9.133431D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =  2322
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  1.952427D+11, CYCLES =  7.032465D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =  1979
 *** USER INFORMATION MESSAGE 5010 (LNCILD)
     STURM SEQUENCE DATA FOR EIGENVALUE EXTRACTION.
     TRIAL EIGENVALUE =  2.468851D+11, CYCLES =  7.908017D+04 NUMBER OF EIGENVALUES BELOW THIS VALUE =  2126
 *** SYSTEM FATAL MESSAGE 3034 (LNNHERR)
     INTERNAL FAILURE IN THE LANCZOS PROCEDURE:
     M-ORTHOGONAL QR PROCEDURE FAILED TO CONVERGE.  PROBABLE CAUSE:
     MASS MATRIX IS INDEFINITE (MODES) OR STIFFNESS MATRIX IS INDEFINITE (BUCKLING).
     USER ACTION: CONTACT SIEMENS PLM SOFTWARE CUSTOMER SUPPORT.
 *** SYSTEM FATAL MESSAGE 7340 (LNNHERR)
     WARNING REPORTED BY SUBROUTINE LNNDRVD  (IER=   728)
     USER INFORMATION:  GRAM-SCHMIDT DID NOT CONVERGE.
 *** SYSTEM FATAL MESSAGE 5407 (LNCCKD)
     INERTIA (STURM SEQUENCE) COUNT DISAGREES WITH THE NUMBER OF MODES ACTUALLY COMPUTED IN A (PARTIAL) INTERVAL
    FOUND    215 MODES BETWEEN  3.0444771E+04 HZ AND  4.0392281E+04 HZ BUT THERE SHOULD BE ONLY    194 MODES.
    FOUND    227 MODES BETWEEN  4.0392281E+04 HZ AND  5.2731889E+04 HZ BUT THERE SHOULD BE ONLY    222 MODES.
    FOUND    319 MODES BETWEEN  5.2731889E+04 HZ AND  7.0324649E+04 HZ BUT THERE SHOULD BE ONLY    295 MODES.
    THIS RUN IS TERMINATED. PARAM,BAILOUT,-1 MAY BE USED TO CONTINUE THE RUN.

    USER ACTION:  THE FOLLOWING CHANGES TO THE EIGRL CARD MAY HELP TO SOLVE THIS PROBLEM
                  1.  INCREASE MAXSET.
                  2.  IF F1 IS GIVEN AS ZERO, LEAVE IT BLANK.
                  3.  IF F1 AND F2 ARE BOTH GIVEN, LEAVE F2 BLANK AND SPECIFY A VALUE FOR ND.


 

1 REPLY

Re: FATAL error in SOL112 run

Experimenter
Experimenter

Hi All,

 

I am able to solve without any errors by  setting PARAM,RESVRAT,1.0e6.