Cancel
Showing results for 
Search instead for 
Did you mean: 

Fluid Effects

Hello there, Is there any tutorial or example on how to fluid effects? Tutorial video would be great. Thanks.

6 REPLIES

Re: Fluid Effects

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi,

 

If you are looking for wet vibration modes you can easily google the topic, i.e. 

https://www.google.de/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&ved=0CB8QFjAA&url=http%3A%2F%2Fhrcak....

 

on top of that your local representative would be able to provide you an example

 

regards, Pavel 

Re: Fluid Effects

Let say i have a boat on the top of the water surface, and then i want apply load to the boat. i want to see the excitation of the boat and water. how to model the water and define interaction between boat hull and water surface? appreciate if you could enlight me on this problem. thanks.

Re: Fluid Effects

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hey,

 

Do you want to directly model waves, sloshing, and another FSI effects?

 

Regards

Pavel

Re: Fluid Effects

Yes. Can Femap with NX Nastran do this kind of analysis? Do i need to add certain features to perform this kind of analysis?

Re: Fluid Effects

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Well in this case I believe the unswer is NO.

 

Btw NX CAE can do part of what you need. 'Manual' FSI based on mapping could be performed, sloshing problem with waives initiated by acceleration can be performed. Some other effects and phenomena. However direct FSI analysis is under development for NX CAE MultiPhysics Application.

 

 

Regards

Pavel

Re: Fluid Effects

I see. Thanks for your answer. Really appreciate your cooperation.