Cancel
Showing results for 
Search instead for 
Did you mean: 

How to increase the Increment in the result

Experimenter
Experimenter

 Dear All,

 

How can I increase the INCREMENT in the result after simulated model?

 

In the attachment, it showed the maximum of Increment is 12, but I wish to make the load press the structure till the end of the tube.

 

Is that available in NX? If yes, how to make it?

 

Thank you.

3 REPLIES

Re: How to increase the Increment in the result

selex_ct 1st Gear
1st Gear

you end up with 12 increment because that's what you requested!

to crush the tube then you need to apply a much larger force but one usually use forced displacement for such problem. You will most likely end up with analysis "difficulty" becuase of self-contact, large stress/strain, etc

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: How to increase the Increment in the result

Experimenter
Experimenter

Thanks for your advice...
So, what should I do? does any guidance steps or demo video available to refer? Because I not familiar with the

Currently, I'm using NX10 on academic purpose, and I'm not familiar with this software yet. Hope somebody can help me...

Re: How to increase the Increment in the result

selex_ct 1st Gear
1st Gear

if not familar with the software then I can only recommend starting with an (easy) problem. Starting with the problem described is not the easiest. No even sure if an academic licence can handle such problem - don't knwo the limitatin of such licence

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)