Cancel
Showing results for 
Search instead for 
Did you mean: 

How to plot a spring characteristic

Experimenter
Experimenter

Hello,

 

I simulated a flat spring with the linear solution 101. Now I want to plot the spring characteristic, force/way diagram. Anyone an idea how I get out the reactionforce over the major displacement of the spring?

 

Thanks

4 REPLIES

Re: How to plot a spring characteristic

Siemens Phenom Siemens Phenom
Siemens Phenom

First you would need to run a solution that produces output at multiple steps. Linear statics outputs a single set of results for each subcase. If you are using NX for pre/post, then you can generate a force-displacement XY graph through its 2 function graph capabilities from the XY Function Navigator. You do this by creating force and displacement graphs separately, then using them together. So, if you have results over time, you would create a force-time graph, followed by a displacement-time graph. Then select both resulting AFU records in the XY function navigator and use the 2 function graph command create a force-displacement graph from the time dependent functions.

 

Regards,

Mark

 

Mark Lamping

Simulation Product Management

Simulation and Test Solutions

 

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

 

mark.lamping@siemens.com

www.siemens.com/plm

Re: How to plot a spring characteristic

Experimenter
Experimenter

thanks for your answer, which solution would you suggest to realize it? 

Re: How to plot a spring characteristic

Siemens Phenom Siemens Phenom
Siemens Phenom

To produce a graph of reaction force or displacements, you need multiple steps/iterations that show the progression of the load. I took your linear static solution and essentially subdivided it into 4. For each subcase I defined an enforced displacement that was 25, 50, 75, and then 100% of the full displacement in your original model. This gives me 4 sets of results. I then defined results probes that were the weighted average displacement and reaction force for the face where the enforced displacement is defined. This gives me a single force and displacement result at each subcase. I then graphed those probes to get results across the subcases.

 

1. Displacement vs. subcase

2. Reaction force vs. subcase

 

To create the Displacement vs. Reaction Force graph, I needed to save those graphs to AFU files. I opened the AFU in the XY Function Navigator and used the Two Function graph command (select 2 records and MB3 Two Function) to produce the Displacement vs. Reaction Force graph.

 

If you expect nonlinear behavior, then you will have to set up something similar using one of the nonlinear solutions.

 

Regards,

Mark

Re: How to plot a spring characteristic

Experimenter
Experimenter
thanks for your time, more than helpful.