Cancel
Showing results for 
Search instead for 
Did you mean: 

How to solve mesh issue? Some nodes are out of area

Creator
Creator

Hi all,

 

I am struggling with the mesh of an area: I've previously applied a divide_face to define the region where I will apply the load later on.

 

In the view of the results obtained, the issue seems to be that the corner of that inner area is confused with the corner of the outer area:Polygon body containing the inner square where I want to apply the loadPolygon body containing the inner square where I want to apply the loadResult of the meshing: some nodes are far away from its theoretical positionResult of the meshing: some nodes are far away from its theoretical position

Has anybody had this kind of issue? Any tip or suggestion to correct this?

 

Thank you in advance,

1 REPLY
Highlighted

Re: How to solve mesh issue? Some nodes are out of area

Phenom
Phenom

It's some sort of "corrupted" geometry. May need to do a 'Recreate and Update' on the faulty bodies. see attached

 

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)