Cancel
Showing results for 
Search instead for 
Did you mean: 

NX NASTRAN Surface to Surface contact problem

Creator
Creator

Hello everyone. I am doing a problem where I have a cylinder and two plates.I need to find out the deformation of the cylinder.I have given the BC and also have given surface to surface contact to cylinder and the plates.

 

But when I run the simulation, the cylinder is penetrating the plates which should not happen.Smiley Frustrated

 

new_sim1.png

 

 

Can any one please help me out.I have attached the sim file for your reference.

 

Actually it should look something like this but for me its penetrating into the plates.

 

Screenshot 2015-08-19 23.32.29.png

 

Waiting for your valuable replies.

2 REPLIES

Re: NX NASTRAN Surface to Surface contact problem

Siemens Phenom Siemens Phenom
Siemens Phenom
  1. Please avoid cross posting the same question in multiple forums.

    http://community.plm.automation.siemens.com/t5/NX-CAE-Forum/NX-NASTRAN-Surface-to-Surface-contact-pr...
  2.  

  3. A .sim file by itself cannot be opened. The parent .fem must also be supplied
  4.  

  5. It looks like the displacements in your post display are scaled. Deformed contact results typically only make sense if the deformation scale factor is 1.0 absolute.

Re: NX NASTRAN Surface to Surface contact problem

Creator
Creator

Sorry Sir for making same post.Next time I will see to that.I have attached my fem and part file.

 

Please do take a look.

 

Thank you for the reply.