cancel
Showing results for 
Search instead for 
Did you mean: 

NX Nastran Help needed

Creator
Creator

My name is Harsh Bhatt.I am new to nastran and I need to do below mentioned problem in the same.

 

My problem has two plates,one moving and one is fixed.There is a plastic cylinder betwwn the two and presuure is acting on both the sides of cylinder and also on the two plates.

 

When I am running the simulation I am not getting the exact result which I should get[Deformation of the cylinder]. My project detail [2D].

 

Screenshot 2015-07-16 15.20.57.png

 

 

Here in 3D

 

Screenshot 2015-07-16 15.26.59.png

 

Please help me.....Waiting for the valuable reply.

3 REPLIES

Re: NX Nastran Help needed

Creator
Creator

Anyone pls help me out

Re: NX Nastran Help needed

Community Manager Community Manager
Community Manager

It seems your problem is in 2D, is there a reason you're modeling it in 3D?


Regards,
Ganesh

Simcenter 3D Community Manager
Simulation and Test Solutions

Re: NX Nastran Help needed

Creator
Creator

Thank you for the reply sir.

 

Actually I dont have any idea about 2d.....

 

It is a dry gas seal.