Cancel
Showing results for 
Search instead for 
Did you mean: 

NX.Nastran and multiprocessing

Creator
Creator
Good morning,
I wonder if NX.Nastran v7.0 can use multiple processors. If yes, how must I setup it? I thought it is enough to specify NPROC=4. But when looking in the Windows Task manager on the power, only about 25pct of the CPU power is used during the analysis. Is this normal? I list the Nastran .log-file below.
My computer is DELL with processor Intel(R) Xeon(R) CPU E5420 @ 2.50GHz having 4 cores. 8 GB RAM. My models have about 1,000,000 nodes, with 3D-elements have 3 DOF per node.

Many thanks for Your answer and help
Regards, Johannes


NX Nastran V7.0 (Intel64 Family 6 Model 23 Stepping 10 Windows Vista Service Pack 1) Control File:
-------------------------------------------------------------------
$Buffsize=8193 $(c:/prog/femapv1011/nastran/conf/nast7.rcf)
$Memory=3000Mb $(c:/prog/femapv1011/nastran/conf/nast7.rcf)
Nastran BUFFSIZE=32769 $(c:/prog/femapv1011/nastran/conf/nast7.rcf)
$msgbell=no $(c:/prog/femapv1011/nastran/conf/nast7.rcf)
Nastran REAL=2143289344 $(program default)
JID='f:/10_ze_1/fe_1/m10_lc_press2bar_templci_stat.bdf'
OUT='./m10_lc_press2bar_templci_stat'
MEM=285972480
MACH='Intel64 Family 6 Model 23 Stepping 10'
OPER='Windows Vista'
OSV='Service Pack 1'
MODEL='Intel(R) Xeon(R) CPU E5420 @ 2.50GHz (DELLE)'
CONFIG=8666
NPROC=4
symbol=DELDIR='c:/prog/femapv1011/nastran/nxn7/nast/del' $(program default)
symbol=DEMODIR='c:/prog/femapv1011/nastran/nxn7/nast/demo' $(program default)
symbol=SSSALTERDIR='c:/prog/femapv1011/nastran/nxn7/nast/misc/sssalter' $(program default)
symbol=TPLDIR='c:/prog/femapv1011/nastran/nxn7/nast/tpl' $(program default)
SDIR='f:/m10_lc_press2bar_templci_stat.T24660_27'
DBS='f:/m10_lc_press2bar_templci_stat.T24660_27'
SCR=yes
NEWDEL='c:/prog/femapv1011/nastran/nxn7/em64tnt/SSS'
DEL='NXNDEF'
AUTH='28000@LocalHost'
AUTHQUE=0
MSGCAT='c:/prog/femapv1011/nastran/nxn7/em64tnt/analysis.msg'
MSGDEST='f06'
PROG=FEMAP
-------------------------------------------------------------------
NXN_ISHELLPATH=C:\Prog\FEMAPv1011\nastran\bin
NXN_JIDPATH=
PATH=c:/prog/femapv1011/nastran/nxn7/em64tnt;c:/prog/femapv1011/nastran/nxn7/em64tnt/mpi/bin;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Program Files (x86)\Common Files\Roxio Shared\DLLShared\;C:\Program Files (x86)\Common Files\Roxio Shared\9.0\DLLShared\;C:\Program Files (x86)\GNU\GnuPG;C:\Prog\FEMAPv1001\nastran\bin;C:\Prog\Aster\Python24
Command Line: JID=F:\10_Ze_1\FE_1\M10_LC_Press2bar_TempLCI_stat.BDF
Current Dir: F:\10_Ze_1\FE_1
Executable: c:/prog/femapv1011/nastran/nxn7/em64tnt/analysis.exe
NXN_MSG: stderr
FPE: no
-------------------------------------------------------------------
Current resource limits:
Physical memory: 8188 MB
Physical memory available: 3839 MB
Paging file size: 16568 MB
Paging file size available: 11886 MB
Virtual memory: 8388607 MB
Virtual memory available: 8388554 MB
-------------------------------------------------------------------
System configuration:
Hostname: DELLE
Architecture: em64tnt
Platform: Intel64 Family 6 Model 23 Stepping 10 Windows Vista Service Pack 1
Model: Intel(R) Xeon(R) CPU E5420 @ 2.50GHz
Clock freq.: 2493 MHz
Number of CPUs: 4
Executable: standard
Raw model ID: 8666
Config number: 8666
Physical memory: 8188 MB
Virtual memory: 16568 MB
Numeric format: 32-bit little-endian IEEE.
Bytes per word: 4
Disk block size: 512 bytes (128 words)
Remote shell cmd: Remote capabilities not available.
-------------------------------------------------------------------
NX Nastran started Thu Nov 4 18:15:35 MZ 2010
18:15:35 Beginning Analysis

18:15:35 NX NASTRAN Authorization Information - System Attributes
18:15:35 --------------------------------------------------------
18:15:35 Model: Intel(R) Xeon(R) CPU E5420 @ 2.5
18:15:35 Machine: Intel64 Family 6 Model 23 Steppi
18:15:35 OS: Windows Vista
18:15:35 Version: Service Pack 1
18:15:35 License File(s): 28000@LocalHost

18:15:35 The FEMAP dll Search String is c:\prog\femapv1011\auth_*.dll .
18:15:35 Found the FEMAP authorization dll auth_101.dll
18:15:35 Loading FEMAP Authorization dll auth_101.dll

18:15:36 NX NASTRAN Authorization Information - Checkout Successful
18:15:36 ----------------------------------------------------------
18:15:36 License for module NX Nastran Basic - FEMAP Desktop checked out successfully

18:16:03 Analysis started.
18:16:03 Geometry access/verification to CAD part initiated (if needed).
18:16:03 Geometry access/verification to CAD part successfully completed (if needed).
18:16:57 Finite element model generation started.
18:24:12 Finite element model generated 4679946 degrees of freedom.
18:24:12 Finite element model generation successfully completed.
18:24:12 Application of Loads and Boundary Conditions to the finite element model started.
18:25:39 Application of Loads and Boundary Conditions to the finite element model successfully completed.
20:51:51 Solution of the system equations for linear statics started.
21:10:53 Solution of the system equations for linear statics successfully completed.
21:11:27 Linear static analysis completed.
21:11:27 NSEXIT: EXIT(0)
21:11:27 Analysis complete 0
Real: 10552.385 seconds ( 2:55:52.385)
User: 8192.954 seconds ( 2:16:32.954)
Sys: 272.471 seconds ( 0:04:32.471)
NX Nastran finished Thu Nov 4 21:11:27 MZ 2010
11 REPLIES

Re: NX.Nastran and multiprocessing

Innovator
Innovator
hello!,
Of course, NX NASTRAN supports multiprocessing, is part of the system, and do not need to pay to support for additional processors like another FEA codes, the price of NX NASTRAN is the same o run models with FOUR CORES or EIGHT CORES, this is important.

But you need to activate multiple cores, if not only ONE core is used. Basically you need to use a NASTRAN KEYBOARD "PARALLEL=4" in case you have a QUAD CORE processor, etc..

The following pictures shows how to activate multiprocessing support in both FEMAP & NX ADVANCED SIMULATION.

Best regards,
Blas.

Re: NX.Nastran and multiprocessing

Creator
Creator
Now it works, thank You for Your help, Johannes

Re: NX.Nastran and multiprocessing

Creator
Creator
I can't see the pictures you postet, blas. have they been deleted?

Re: NX.Nastran and multiprocessing

Innovator
Innovator
Dear Renk,
Here you have the pictures again.
Best regards,
Blas.

Re: NX.Nastran and multiprocessing

Creator
Creator
Thanks a lot, blas!

Re: NX.Nastran and multiprocessing

Is there a way to make this setting permanent?
I have tried to add the string "PARALLEL=4" in Customer Defaults--->Simulation--->NASTRAN--->Solver Parameters--->Additional Keywords but it doesn't work.
If I open the Solver Parameters window from Solve--->Edit solver parameters the Additional Keywords field is blank and if I run the analisys only the 25-30% of processors is used on my quad-core workstation.

Re: NX.Nastran and multiprocessing

Siemens Phenom Siemens Phenom
Siemens Phenom
Giuseppe,

I am running NX 7.5.4 and was able to define additional keywords in the customer defaults and get them to show up in new solution sets after I restarted NX. What version of NX are you running?

Regards,
Mark

Re: NX.Nastran and multiprocessing

Mark,
I am running NX 7.5.0.32.
You are right, after the restart the additional keyword is automatically added to new solutions. I thought I should have seen it also on existing sim/solutions.
Thank you,
GC

Re: NX.Nastran and multiprocessing

Innovator
Innovator
Dear Giuseppe,
If you load an old SIM file with a solution where you din't used PARALLEL=4 then you will have to add command PARALLEL=4 by hand, this is not automatic done.
But if you delete the study or create a new one then you will see that PARALLEL=4 is added atomatically, OK?.
Best regards,
Blas.