cancel
Showing results for 
Search instead for 
Did you mean: 

Nonlinear Cbush

Experimenter
Experimenter
Hi,

I'm trying to implement a nonlinear spring constant with a polynominal approach. For Example; c= 165x^3-115x^2+57x+4.

Is this possible? Also in Sol103

Thanks
Michael
1 REPLY

Re: Nonlinear Cbush

Siemens Builder Siemens Builder
Siemens Builder
Nonlinear spring stiffness is defined on PBUSHT using the KN flag. The actual stiffness data is defined on TABLEDi entries, so you would need to discretize your function to generate the data.

Per PBUSHT remarks 5-7, this is only supported in SOL's 106, 129 and 601
--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm