Cancel
Showing results for 
Search instead for 
Did you mean: 

Normal mode shape display in phase

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

from the modal analysis I have normal frequency and mode. The mode (shape) is mostly displayed as displacement, e.g. for simple bar it is bending. And I want to display it in opposite direction as default - in opposite phase. How to get it? Is it a setting of NX Nastran solution or just function of Simcenter post process?

Juraj

3 REPLIES

Re: Normal mode shape display in phase

Phenom
Phenom

animate the mode shape and select the frame in which the part is the "position" you want perhaps

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: Normal mode shape display in phase

Genius
Genius

Setting the deformation scale of the post view to a negative value will flip the phase of the deformed shape. I do not know how to set this as a default so you may need to create a post processing template to quickly apply the format.

Re: Normal mode shape display in phase

Siemens Phenom Siemens Phenom
Siemens Phenom

Specify a negative scale factor on the deformation dialog

 

Deformation =10% of model (Default):

ModeDisp+10.png

 

Deformation = -10%:

 ModeDisp-10.png