Cancel
Showing results for 
Search instead for 
Did you mean: 

Number of eigen values on SOL 103

Experimenter
Experimenter

Hello again. When I do a SOL 103 analysis on NX10.0, where do I define the number of Eigenvalues that I want as a result?

1 REPLY

Re: Number of eigen values on SOL 103

Siemens Phenom Siemens Phenom
Siemens Phenom

In Nastran, this ic controlled by an EIGRL bulk data card referenced by a METHOD card in case control.

 

For a METHOD in the global case, edit the solution in NX. In the Case Control section, define a Lanczos Data Modeling object. This object allows you to define min and max frequency, number of modes, and all other fields on the EIGRL card.

 

For a METHOD in a specific subcase, edit the subcase and select a Lanczos Data modeling object in that location.

 

If a different method is defined in each location, the one defined in the subcase is used for the analysis.