Cancel
Showing results for 
Search instead for 
Did you mean: 

Plotting Stress-Strain curve

Creator
Creator

Hi,

In NX 11, is there a way of plotting the stress strain curve in the results navigator? I am using sol 106 and 601 to solve some non-linear problems, and I would like to have the stress strain curve so that I can compare. 

1 REPLY

Re: Plotting Stress-Strain curve

Siemens Phenom Siemens Phenom
Siemens Phenom

You can create the stress-strain plot using multiple steps. Individually create stress and strain graphs, then use 2 function plot capabilities to get the stress-strain graph.

 

1. Create a stress graph at a given location

2. Create a strain graph at the same location

3. Save both graphs to an AFU file

4. Open the AFU file in the XY Function navigator

5. Select both functions in the XY Function navigator and use the 2 function plot capability

 

You can also do this through stress and strain post processing views. That is described in the following online help article.

 

https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:xid612422

 

Regards,

Mark