Showing results for 
Search instead for 
Do you mean 
Reply

Pre-load a structure

Hello all,
I would like to set up the following configuration in SOL 101.
geometry : beam (100m*20mm*10mm)
3 points bending, both ends of the beam fully constrained.
Apply a -0.15mm enforced displacement at the middle of the beam
Then :
Apply a -Z direction force at the middle of the beam (same nodes than
previously enforced).
Observe the cumulative effect.
So far the added force is not acting as I would like, ie. the enforced
displacement prevents the beam from bending more
than the effect of the displacement value I entered.
I s there a way to set up the simulation so that the following scenario
runs :
Apply a given displacement (could be a force as well), then apply a
force (could be an enforced displacement as well).
I fear this is not solvable as linear.
Thanks in advance,
Tamas

8 REPLIES

Re: Pre-load a structure

Tamas,

You cannot do this as a linear analysis because the constraints are changing between loading conditions.

Regards,
Jim
--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm

Re: Pre-load a structure

Dear Tamas,
This is a nonlinear static analysis, you need to setup a NX NASTRAN SOL106 analysis using subcases, or a SOL601,106 analysis with Time-Varying loads using the concept of "arrival time", this a very typical situation to simulate a non linear buckling analysis: prescribing a nodal displacement a applying a load you get a small deformed shape to account for geometric imperfections and then apply the real loads over the deformed shape to get model response.
Best regards,
Blas.
--
~~~~~~~~~~~~~~~~~~~~~~
Blas Molero Hidalgo
Ingeniero Industrial
Director

IBERISA
Edificio Ercilla
Rodríguez Arias 23, 3º - Dpto. 19
48011 BILBAO (SPAIN)
Tel. (+34) 94 410 65 50
Fax. (+34) 94 470 26 34
E-mail: info@iberisa.com
WEB: http://www.iberisa.com
"Tamas" escribió en el mensaje de noticias news:4b0c12d1$1@bbsnotes.ugs.com...
> Hello all,
>
> I would like to set up the following configuration in SOL 101.
>
> geometry : beam (100m*20mm*10mm)
> 3 points bending, both ends of the beam fully constrained.
>
> Apply a -0.15mm enforced displacement at the middle of the beam
> Then :
> Apply a -Z direction force at the middle of the beam (same nodes than
> previously enforced).
>
> Observe the cumulative effect.
>
> So far the added force is not acting as I would like, ie. the enforced
> displacement prevents the beam from bending more
> than the effect of the displacement value I entered.
>
> I s there a way to set up the simulation so that the following scenario
> runs :
>
> Apply a given displacement (could be a force as well), then apply a
> force (could be an enforced displacement as well).
>
> I fear this is not solvable as linear.
>
> Thanks in advance,
>
> Tamas
>
>

Re: Pre-load a structure

Jim, Blas,
Thanks a lot, I will git it a try.
regards,
Tamas

Blas Molero Hidalgo a écrit :
> Dear Tamas,
> This is a nonlinear static analysis, you need to setup a NX NASTRAN
> SOL106 analysis using subcases, or a SOL601,106 analysis with
> Time-Varying loads using the concept of "arrival time", this a very
> typical situation to simulate a non linear buckling analysis:
> prescribing a nodal displacement a applying a load you get a small
> deformed shape to account for geometric imperfections and then apply the
> real loads over the deformed shape to get model response.
> Best regards,
> Blas.
> --
> ~~~~~~~~~~~~~~~~~~~~~~
> Blas Molero Hidalgo
> Ingeniero Industrial
> Director
>
> IBERISA
> Edificio Ercilla
> Rodríguez Arias 23, 3º - Dpto. 19
> 48011 BILBAO (SPAIN)
> Tel. (+34) 94 410 65 50
> Fax. (+34) 94 470 26 34
> E-mail: info@iberisa.com
> WEB: http://www.iberisa.com
> "Tamas" >
> escribió en el mensaje de noticias news:4b0c12d1$1@bbsnotes.ugs.com...
> > Hello all,
> >
> > I would like to set up the following configuration in SOL 101.
> >
> > geometry : beam (100m*20mm*10mm)
> > 3 points bending, both ends of the beam fully constrained.
> >
> > Apply a -0.15mm enforced displacement at the middle of the beam
> > Then :
> > Apply a -Z direction force at the middle of the beam (same nodes than
> > previously enforced).
> >
> > Observe the cumulative effect.
> >
> > So far the added force is not acting as I would like, ie. the enforced
> > displacement prevents the beam from bending more
> > than the effect of the displacement value I entered.
> >
> > I s there a way to set up the simulation so that the following scenario
> > runs :
> >
> > Apply a given displacement (could be a force as well), then apply a
> > force (could be an enforced displacement as well).
> >
> > I fear this is not solvable as linear.
> >
> > Thanks in advance,
> >
> > Tamas
> >
> >

Re: Pre-load a structure - new question

Hello all,
I tried this morning SOL106 works fine, thanks a lot.
SOL601,106 wouldn't work it seems I don't have the right license file.
Could you please tell me idf with the following lic file I should be
able to perform SOL601,106?

Thanks a lot in advance.
Tamas
VENDOR ugslmd
PACKAGE A026G ugslmd 24.0000 E9DA37B4645A \
COMPONENTS="A026G_ansys_meshers A026G_assemblies \
A026G_features_modeling A026G_gateway A026G_gfem_ansys \
A026G_gfem_nastran A026G_grip_execute A026G_id_ext_fem_beam \
A026G_iges A026G_nx_freeform_1 A026G_nx_freeform_2 \
A026G_nx_ftk A026G_nx_masterfem A026G_nx_material_system \
A026G_pcf_package_file A026G_pstudio_cons \
A026G_pv_ugdatagenerator A026G_sla_3d_systems \
A026G_solid_modeling A026G_studio_render \
A026G_studio_visualize A026G_ug_checkmate A026G_ug_collaborate
\
A026G_ug_kf_checker A026G_ug_kf_execute A026G_ug_scenario \
A026G_ug_smart_models A026G_ug_web_express \
A026G_ugopen_menuscript A026G_usr_defined_features" \
OPTIONS=SUITE ck=149 SIGN="104E 9447 71D2 8B37 7841 55D5 A44F \
1750 52D5 B05A D751 6F25 8B35 94DF BDEF 0748 95AC 766E 07E1 \
062B E901 C56A 0400 163D 7256 3A7B 6178 AAFD EE0B E82C"
INCREMENT 3d_to_2d_flattener ugslmd 24.0 permanent 1 BA3D677398FB \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=131 SIGN="07BD \
F566 90D1 2D6A EAF9 0C95 8B8A C60B 9388 D24E 14FB 55DA 55E6 \
076A 87F3 121F D6DB F090 B7EE A7F4 A5F1 6312 6A91 3373 C948 \
941D A799 49C3 4BD1 4B16"
INCREMENT A026G ugslmd 24.0 permanent 1 58E9F08D26EC SUPERSEDE \
DUP_GROUP=UHD user_info=MasterFEM ISSUED=17-jul-2008 ck=177 \
SIGN="08CC 2895 1C3A 96C3 F45F 6A9F E236 E9E5 E7FB 10E1 34A7 \
5BE4 E651 99F4 3B0C 16A7 808E D5E0 8BF8 49B2 2C9E D80A 5FEE \
F25E B245 E3A5 42E1 D780 6BCC D471"
INCREMENT drafting ugslmd 24.0 permanent 1 F2CF1333738A SUPERSEDE \
DUP_GROUP=UHD ISSUED=17-jul-2008 ck=110 SIGN="02AF E7CE 1252 \
6DC1 0496 020B FCB7 ACA9 1C48 114B BAE3 EBAB 041C D0DD FE8E \
0799 F853 AF23 E903 698A E813 C093 96D1 04C6 7384 DE19 E080 \
9D07 8C74 D013"
INCREMENT dxfdwg ugslmd 24.0 permanent 1 47808E7D8CCC SUPERSEDE \
DUP_GROUP=UHD ISSUED=17-jul-2008 ck=131 SIGN="1EAF B27F 28DC \
52F0 B314 A957 B0F5 EEBB 783E C30E F59D 1699 3560 7BB8 9EC1 \
05B5 6774 7C7E BBD4 1DA3 48A1 E550 DC1C 8ED8 9FAA 08BC 3772 \
DCE8 EC1A 7BCD"
INCREMENT features_modeling ugslmd 24.0 permanent 1 C7CA6791A861 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=126 SIGN="1672 \
8914 8985 983C 2B57 03E2 CA09 1F95 C22F 47D2 C090 16EA F329 \
BFD5 CFE7 04F3 013C 25C6 7549 1300 3137 195B 7E76 BE21 4AB4 \
5848 A6B2 6B54 027F FD8E"
INCREMENT gateway ugslmd 24.0 permanent 2 B05B60F44A65 SUPERSEDE \
DUP_GROUP=UHD ISSUED=17-jul-2008 ck=69 SIGN="05A0 0C66 33FB \
5380 C187 E225 8629 A453 AFFD 1A3D 5281 3FC6 7A12 E2DF 9B8B \
0CC3 A4AD 700F 6DD7 B399 B1FE 73FE 52B6 9D1B A935 D4EF 8775 \
E596 B555 5362"
INCREMENT geometric_tol ugslmd 24.0 permanent 1 0A4B01AF7548 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=50 SIGN="1A0F \
C8CD 1773 8838 2129 0638 F8D1 A0FC EE10 284B D399 7356 7F02 \
21DD 8437 07BE 1227 D0F6 E696 89D0 5199 37B5 DF2E 8592 C770 \
30A9 37BE 325F 46E1 9DC7"
INCREMENT iges ugslmd 24.0 permanent 2 8D71E4BF6ABF SUPERSEDE \
DUP_GROUP=UHD ISSUED=17-jul-2008 ck=192 SIGN="1459 E5AD 4BE1 \
BF15 DC87 133F 0730 DEDE F720 37F8 AB47 B938 B2DE 9E2E E585 \
1DA9 E635 84CE 19C7 24E8 8C70 7D5E 9C32 364E 5C3F 209F 8578 \
A2F2 BE45 06FB"
INCREMENT nx_freeform_1 ugslmd 24.0 permanent 1 EA34BC55FADA \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=147 SIGN="0BC0 \
3941 91E7 E43F 1A06 E477 6F9F C206 FA17 8794 E3A1 4ADA E482 \
B548 2E13 0612 F789 7FB2 7F6E 57E6 B698 7413 9B6D D559 F5F8 \
271F 87B4 D546 C206 D575"
INCREMENT nx_freeform_2 ugslmd 24.0 permanent 1 3D24AE5211D4 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=97 SIGN="0E16 \
3E57 84F1 E2CB FA6B 464E AD5F 8620 6EE7 11B6 18A0 245D 1CB6 \
1B86 350D 0A8F 04C1 EA5A 96D5 778F 5FED 9576 391B AAF4 90DB \
67E8 9583 030F 9E81 6B03"
INCREMENT nx_material_system ugslmd 24.0 permanent 1 01561A8E4A61 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=133 SIGN="198B \
A93D C830 0898 DB21 ED53 5E07 CF97 54C9 F56D FA3A E591 15B1 \
05D5 0EEB 0547 CACD CAFB 999D E0B8 2E52 351B A49E A901 7B7E \
083F E5B9 20DF E11A 1909"
INCREMENT nx_nas_basic_dsk ugslmd 24.0 permanent 1 1C6793F9F6B6 \
SUPERSEDE DUP_GROUP=NONE ISSUED=17-jul-2008 ck=153 SIGN="18A2 \
0C3B A04E CFE3 7249 8708 8E15 4052 B422 E169 C457 67CF 5147 \
8BC8 C324 0534 FAFD 9DDC 5C69 B246 4E89 9ADC 3BDA D09B 6DEC \
6BDA 3A08 1CAB 5059 E5DC"
INCREMENT nx_nas_nonlin_dsk ugslmd 24.0 permanent 1 432167C4C06A \
SUPERSEDE DUP_GROUP=NONE ISSUED=17-jul-2008 ck=71 SIGN="0842 \
4036 65B8 BA33 4744 F021 8CEC BD9F B06A B6FE DA72 0C8D B771 \
4EA9 B038 0563 AE78 D01B 32EE E210 BF6D 4F49 32AF 125A B4A9 \
CEBF E770 9516 7F19 AD05"
INCREMENT nx_nastran_export ugslmd 24.0 permanent 1 5CCC2D4E9004 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=134 SIGN="01B1 \
111E 9F3F C0B5 6BF7 00FC 2CB5 3FEE 0F7D CDE2 5897 B945 F62F \
72DB FADD 1E3A AC25 162D E724 26C0 97A2 EAFA EABE 92A3 CFBE \
E592 70EB 4564 3444 DA25"
INCREMENT nx_nastran_import ugslmd 24.0 permanent 1 5117A871B3C8 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=67 SIGN="0DDA \
59D2 941B 92BE B1DF 6658 4345 0FC8 7641 98AE B5B5 9E22 7C3D \
FE81 D43F 07A2 6F00 E456 7136 004F EE49 CC32 0CB1 DFB6 2095 \
13CC 857A 40C2 27AC A241"
INCREMENT nx_response_anlys ugslmd 24.0 permanent 1 BF1D0715D519 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=85 SIGN="0B88 \
6F27 5516 7CAA 5DD9 E4E2 A012 1B91 1F36 26C3 BC5D A93A 932F \
C76C 4222 07BC B878 0FFB 4CB6 BE7E 0B17 D3D8 A9DC 2C4B 2D15 \
06A5 6A04 67E1 0001 9722"
INCREMENT pstudio_cons ugslmd 24.0 permanent 2 7B9038B51CB3 SUPERSEDE \
DUP_GROUP=UHD ISSUED=17-jul-2008 ck=56 SIGN="1030 0169 4F8C \
B3CC 9897 0CDF DEB1 B0DC 251B 7F1F 75F0 75D7 B49D 6B5A 58B4 \
0D3D AB8B E5CF 9C38 C349 C33D 0E1D 8FF6 FC7B 0BB4 3BFC D149 \
9845 D315 3CB3"
INCREMENT pv_ugdatagenerator ugslmd 24.0 permanent 2 C349DE30A378 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=103 SIGN="12BF \
0015 DA14 D63B 345D 7F12 967B 90E0 7F59 BBFB 330E 4955 1A14 \
71ED 7FA9 1806 3D1F B220 7E2B 9543 DB4F AB47 8B45 B9E8 7F0B \
735A 5725 C8D4 F604 86E3"
INCREMENT sla_3d_systems ugslmd 24.0 permanent 1 FA5963E06B12 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=68 SIGN="1EA8 \
D115 E7D2 6C3C FF78 8D63 ECC1 6517 F3FC 4ABE 8896 116B 40D6 \
0F24 76CF 164D 38FE BC48 6652 1A73 EE55 FB76 8A02 19E3 4104 \
769C 0669 7DAF F215 967F"
INCREMENT solid_modeling ugslmd 24.0 permanent 1 B1BD4BE7FC3C \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=159 SIGN="14AD \
64F9 DC4E CAC2 C8CC 2507 177E 956D 9B4A 122F 8B68 0DB5 09D8 \
351B 5C46 0A33 9A26 663C 7CE0 3677 FAB1 E412 EA1E 3B1E 2F22 \
B4C5 58EA DA46 58C9 CAEA"
INCREMENT ug_collaborate ugslmd 24.0 permanent 2 5B7767A7A864 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=101 SIGN="0781 \
8439 BF19 4FAA 2462 6795 7023 F668 5E93 A62B A266 52C3 7CB2 \
47E7 3BB5 1EA9 19C1 BC88 B25C 75CC 8E00 862C 94AF 6E8E F902 \
6EF1 B86F 957D 982A 336E"
INCREMENT ug_smart_models ugslmd 24.0 permanent 2 CFCF88372439 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=92 SIGN="0B0F \
3677 A0C2 6718 F4E9 B8B7 2192 2578 4351 E042 4785 8CB9 2F8A \
5921 7628 0EF9 688F CE1E FC6F A96E 9824 0580 9720 EFDA 61C0 \
E159 2A3E BDE3 D409 8EAF"
INCREMENT ug_struct_pe_solver ugslmd 24.0 permanent 1 C371755530F3 \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=141 SIGN="141B \
2FB9 763D 1DA1 01A7 6B82 3B0E D043 B306 D5D2 7845 D32A D09A \
24C8 C8F6 0696 1F39 A797 36BF 1779 9D15 6D74 C1A0 0FBC 1104 \
7BFE 56FC CB88 9AFC 3883"
INCREMENT ugopen_menuscript ugslmd 24.0 permanent 2 5AE80211A22E \
SUPERSEDE DUP_GROUP=UHD ISSUED=17-jul-2008 ck=86 SIGN="1DE9 \
EAAE 2164 971B D8D0 6E6C 4691 CEBB E37C F1E6 21AB C0FF BD86 \
D096 D669 0ADE 4517 72A1 2CA1 6711 A662 2B1E D4D3 1965 DB73 \
84B8 5C33 7918 1921 9302"
FEATURE server_id ugslmd 24.0 permanent 1 2CC424E6F2B6 \
VENDOR_STRING="64335 - HITCHINER France" user_info=QXGFFMW604 \
ISSUER=UGS ck=125 SIGN="10D0 F739 59B8 56F9 F02C A9D8 4F8E \
C101 589F EB47 6419 0095 BC75 AE5B 5DD6 185F 08B5 A317 B16B \
213F 6DEB 7082 F9F1 46B1 687B B369 921B E019 DE4D 191A"


Tamas a écrit :
> Jim, Blas,
>
> Thanks a lot, I will git it a try.
>
> regards,
> Tamas
>
>
>
> Blas Molero Hidalgo a écrit :
>> Dear Tamas,
>> This is a nonlinear static analysis, you need to setup a NX NASTRAN
>> SOL106 analysis using subcases, or a SOL601,106 analysis with
>> Time-Varying loads using the concept of "arrival time", this a very
>> typical situation to simulate a non linear buckling analysis:
>> prescribing a nodal displacement a applying a load you get a small
>> deformed shape to account for geometric imperfections and then apply
>> the real loads over the deformed shape to get model response.
>> Best regards,
>> Blas.
>> --
>> ~~~~~~~~~~~~~~~~~~~~~~
>> Blas Molero Hidalgo
>> Ingeniero Industrial
>> Director
>>
>> IBERISA
>> Edificio Ercilla
>> Rodríguez Arias 23, 3º - Dpto. 19
>> 48011 BILBAO (SPAIN)
>> Tel. (+34) 94 410 65 50
>> Fax. (+34) 94 470 26 34
>> E-mail: info@iberisa.com
>> WEB: http://www.iberisa.com
>> "Tamas" >
>> escribió en el mensaje de noticias news:4b0c12d1$1@bbsnotes.ugs.com...
>> > Hello all,
>> >
>> > I would like to set up the following configuration in SOL 101.
>> >
>> > geometry : beam (100m*20mm*10mm)
>> > 3 points bending, both ends of the beam fully constrained.
>> >
>> > Apply a -0.15mm enforced displacement at the middle of the beam
>> > Then :
>> > Apply a -Z direction force at the middle of the beam (same nodes than
>> > previously enforced).
>> >
>> > Observe the cumulative effect.
>> >
>> > So far the added force is not acting as I would like, ie. the enforced
>> > displacement prevents the beam from bending more
>> > than the effect of the displacement value I entered.
>> >
>> > I s there a way to set up the simulation so that the following

>> scenario
>> > runs :
>> >
>> > Apply a given displacement (could be a force as well), then apply a
>> > force (could be an enforced displacement as well).
>> >
>> > I fear this is not solvable as linear.
>> >
>> > Thanks in advance,
>> >
>> > Tamas
>> >
>> >

Re: Pre-load a structure

You do not have a license to run SOL 601. You need to purchase the NX Nastran Desktop Advanced Non-Linear product (NXN120) to run SOL 601 or SOL 701.

Regards
Mark

Re: Pre-load a structure

That my guess too.
Thanks anyway.
regards,
Tamas
zzyl90 a écrit :
> You do not have a license to run SOL 601. You need to purchase the NX
> Nastran Desktop Advanced Non-Linear product (NXN120) to run SOL 601 or
> SOL 701.
>
> Regards
> Mark
>
>

Re: Pre-load a structure - new question

Tamas,

The license file you attached contains the following 2 NX Nastran features:

nx_nas_basic_dsk
nx_nas_nonlin_dsk

You need an nx_nas_advnlin_ feature to run Advanced Nonlinear (SOL 601)

Regards,
Jim
--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm

Re: Pre-load a structure

Hello Jim,
That's what I thought, thanks.
regards,
Tamas
tsbernar a écrit :
> Tamas,
>
> The license file you attached contains the following 2 NX Nastran
> features:
>
> nx_nas_basic_dsk
> nx_nas_nonlin_dsk
>
> You need an nx_nas_advnlin_ feature to run Advanced Nonlinear (SOL
> 601)
>
> Regards,
> Jim
>
>