Cancel
Showing results for 
Search instead for 
Did you mean: 

Print rotation SOL 601,129

Creator
Creator

Hello,

 

I would like to know how I can output the rotations of the node for the SOL601,129. 

I get the translation, but the rotational dof are all zero.

 

Thanks

2 REPLIES

Re: Print rotation SOL 601,129

Siemens Phenom Siemens Phenom
Siemens Phenom

If the grid you are printing displacements for is only attached to a solid element, it will only have 3 translational reaction forces. Solid elements only provide translational stiffness.

 

If the grid is attached to shells, beams, rigids, etc, then there will be translational and rotational reactions.

Re: Print rotation SOL 601,129

Creator
Creator

Thank you for your answer.

 

But I am using CTRIA3 element that are shells. I am simulating a cantilever plate with enforced displacement and rotations at its root.

I have all 6DOF reaction forces. But the rotations (exept for the constrained nodes in which I have assigned a rotation) are zero.

 

This is part of my input file.

 

=========================

INIT MASTER(S)
NASTRAN SYSTEM(442)=-1, SYSTEM(319)=1
ASSIGN OUTPUT2='advnlin.op2',UNIT=21
ID DaPresen,Femap
SOL 601,129
TIME 10000
CEND
ECHO = NONE
DISPLACEMENT(SORT1,PLOT) = ALL
ACCELERATION(SORT1,PLOT) = ALL
SPCFORCE(SORT1,PLOT) = ALL
GPFORCE(SORT1,PLOT) = ALL
ELSTRAIN(SORT1,PLOT) = ALL
DLOAD = 1
SPC = 1
IC = 1
TSTEP = 1
BEGIN BULK
$ Parameters for SOLs 601
PARAM,LGDISP,1
$ Parameters for SOLs 129
PARAM,AUTOSPC,NO
PARAM,GRDPNT,0
PARAM,OGEOM,NO
PARAM,POST,-1
PARAM,PRGPST,YES

$ Strategy Parameters for SOLs 601 and 701
NXSTRAT 1 SOLVER 0 AUTO 0 NPOSIT 0
+ MASSTYP 0 TINTEG 0 ALPHA 0.25
+ DELTA 0.5

===========================