Cancel
Showing results for 
Search instead for 
Did you mean: 

Requirements (memory) disappeared from .f04 file

Creator
Creator

Hi there!

 

The title says it all actually. I am using NX 9.03


I have been looking for the best ways to simulate the bolt connections I need to create.

Since yesterday I noticed something strange. After a few days of modifying the rcf nastran config file I noticed that the 'memory requirements' are gone from the .f04 file. The entire section with requirements is gone.

 

Whatever I do to the rcf file, this section doesn't return.

I was experimenting with NX10 rcf settings like:

"mem=0.45*Physical
Smem=6Gb
Buffsize=65536
parallel=4"

Where I believe the original was something like

"Memory=estimate

Buffsize=8193"

I cannot verify this as I was stupid enough to forget making a backup before I started editing.

 

Can someone help me?

3 REPLIES

Re: Requirements (memory) disappeared from .f04 file

Siemens Genius Siemens Genius
Siemens Genius

Auth=28000@...
Sdir=$TEMP
scr=yes
buffsize=32769
memory=.45*physical
smem=20.0X
buffpool=20.0X
ishellpath=%NXN_BASE%\bin
msgbell=no
fpe=no
diag=8

Re: Requirements (memory) disappeared from .f04 file

Siemens Genius Siemens Genius
Siemens Genius

Of course, please replace the "..." with your server name or physical IP address.

Re: Requirements (memory) disappeared from .f04 file

Creator
Creator

Hi!

 

Thanks for responding!

Unfortunately those are not settings I can use. NX 9 does not seem to understand the 20.0X designation as I get errors every time I use something else than "xGb"