Cancel
Showing results for 
Search instead for 
Did you mean: 

Restart Analysis using NX Nastran Desktop version

N/A

Hello,
i am trying to restart an analysis (the analysis stopped with error of insufficient
time).
i am using NX nastran Desktop version and i need to submit the input deck file from
NX interface.
how can i get to write the input solver file from NX interface without the bulk
data section?
Many thanks,
1 REPLY

Re: Restart Analysis using NX Nastran Desktop version

N/A

"engrequest" wrote:
>
>Hello,
>
>i am trying to restart an analysis (the analysis stopped with error of insufficient
>time).
>i am using NX nastran Desktop version and i need to submit the input deck
>file from
>NX interface.
>how can i get to write the input solver file from NX interface without the
>bulk
>data section?
>
>Many thanks,
>

To make any type of changes (including deleting cards) to the bulk data section
when using a desktop license, you'll need to solve the solution from within NX.
On the Solve form, change Submit to "Write, Edit & Solve Input File" or "Edit Input
File" to edit the existing copy. When you are done editing, save the updated file
from the editor. If you chose "Write, Edit & Solve Input File", the solution should
start as soon as you exit the editor. If you chose "Edit Input File", you need to
go back to the solve form in NX a second time and select "Solve Input File".
Note that NX can launch whatever text editor you prefer for this edit operation
if you specify the path to the editor in the environment variable UGII_EDITOR
Regards,
Jim