Showing results for 
Search instead for 
Do you mean 
Reply

SOL 159 fatal message after adding latent heat

Hi, 

 

I would like to model the effect of latent heat with SOL 159. I added the latent heat of vaporization in the MAT4 card:

 

MAT4 1 6.7000+35.2600+84.4300-6 1.000000 +
+ 660.0000 9.00003.970+11

 

I also used the following TSTEPNL and PARAM cards:

 

BEGIN BULK
$
PARAM,NDAMP,0.1
$
TSTEPNL 100 400.006000 1 2 10 P+
+ 0.0100000.0010001.0000-6 2 10 20.200000 +
+ 9 5 0.750000 16.00000.100000 20.0000 YES+
$

 

I utilized NDAMP to allow for damping. I also increased MAXBIS to 9 to increase the maximum number of bisection step.

 

However I still got the following fatal message:

 

0 N O N - L I N E A R I T E R A T I O N M O D U L E O U T P U T

STIFFNESS UPDATE TIME 0.01 SECONDS SUBCASE 1
ITERATION TIME 0.00 SECONDS

- - - - ERROR FACTORS - - - CONVERGENCE FACTORS - - - LINE SEARCH DATA - - - ITR MAT NO.
TIME ITER DISP. LOAD WORK LAMBDA(I) DLMAG FACTOR E-FIRST E-FINAL NQNV NLS DIV DIV BIS ADJUST

*** USER INFORMATION MESSAGE 6193 (NL2CON)
*** MAXIMUM NUMBER OF BISECTIONS OR MINIMUM TIME STEP HAS BEEN REACHED.
*** USER FATAL MESSAGE 4551 (NL2CON)
*** PREVIOUS MESSAGE HAS OCCURRED ON FIVE CONSECUTIVE TIME STEPS.
^^^ USER INFORMATION MESSAGE 9010 (NLTRAN)
^^^ LAST ADJUSTED DELTA T: OLDDT= 1.953125E-07
^^^ USER INFORMATION MESSAGE 9003 (NLTRAN)
^^^ CURRENT VALUE OF STIME IS 4.326953E-03
^^^ USER INFORMATION MESSAGE 9005 (NLTRAN)
^^^ THE SOLUTION FOR LOOPID= 1 IS SAVED FOR RESTART.

 

If I removed the latent heat property then the solution will proceed fine without the fatal message. Any one has any suggestions? 

 

Thanks!