cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet metal forming analysis

N/A

Hi,
I saw UGS website (http://www.ugs.com/products/nx/docs/fs_nastran_nonlinear.pdf)
shown a sheet metal foeming analysis. I hope to know,
1.Whether this is a permanent deformation or a 'large deformation' which will be
fully reversed back after load released?
2.Is Nastran able to perform such sheet metal forming (permanent) analysis? Where
can I get such related information?
Thanks in advanced.
Best Rgds
Pingshan
3 REPLIES

Re: Sheet metal forming analysis

N/A

Hello Pingshan,
Yes, the NX Nastran Advanced Nonlinear Solver is able to do sheet metal forming
analysis. The material can be represented with nonlinear stress-strain properties
so that plastic deformation occurs and the metal permanently deforms.
The datasheet you cited is the main documentation we have for this solver. If you
need more information, I suggest you contact your sales representative and they
can hook you up to a local support person.
Regards
Mark



"Li Pingshan" wrote:
>
>Hi,
>
>I saw UGS website (http://www.ugs.com/products/nx/docs/fs_nastran_nonlinear.pdf)
>shown a sheet metal foeming analysis. I hope to know,
>
>1.Whether this is a permanent deformation or a 'large deformation' which will
>be
>
>fully reversed back after load released?
>2.Is Nastran able to perform such sheet metal forming (permanent) analysis?
>Where
>
>can I get such related information?
>
>Thanks in advanced.
>
>Best Rgds
>Pingshan

Re: Sheet metal forming analysis

N/A

Hi, Mark
Thank you for the answer.
May I know is this technology being used in the sheet matel stamping process
analysis? Any recommendation for application of this technology?
Best Rgds
Pingshan


"Mark Donley" wrote:
>
>Hello Pingshan,
>
>Yes, the NX Nastran Advanced Nonlinear Solver is able to do sheet metal forming
>analysis. The material can be represented with nonlinear stress-strain properties
>so that plastic deformation occurs and the metal permanently deforms.
>
>The datasheet you cited is the main documentation we have for this solver.
>If you
>need more information, I suggest you contact your sales representative and
>they
>can hook you up to a local support person.
>
>Regards
>Mark
>
>
>
>
>
>
>"Li Pingshan" wrote:
>>
>>Hi,
>>
>>I saw UGS website (http://www.ugs.com/products/nx/docs/fs_nastran_nonlinear.pdf)
>>shown a sheet metal foeming analysis. I hope to know,
>>
>>1.Whether this is a permanent deformation or a 'large deformation' which

>will
>>be
>>
>>fully reversed back after load released?
>>2.Is Nastran able to perform such sheet metal forming (permanent) analysis?
>>Where
>>
>>can I get such related information?
>>
>>Thanks in advanced.
>>
>>Best Rgds
>>Pingshan

>

Re: Sheet metal forming analysis

N/A

Hi Pingshan,
NX Nastran Advanced Nonlinear is an integration of the well known Adina non-linear
solver in the NX Nastran environment. User inputs and outputs are completely Nastran-centric,
but the solver behind the scenes is the Adina solver.
As such this solver is used for a wide range of non-linear solutions and has very
broad applications. Some users do use it specifically for analyzing sheet metal
stamping operations - for applications such as forming an oil-pan or car body/chassis
parts.
Regards
Mark


wrote:
>
>Hi, Mark
>
>Thank you for the answer.
>
>May I know is this technology being used in the sheet matel stamping process
>
>analysis? Any recommendation for application of this technology?
>
>Best Rgds
>Pingshan
>
>
>
>
>"Mark Donley" wrote:
>>
>>Hello Pingshan,
>>
>>Yes, the NX Nastran Advanced Nonlinear Solver is able to do sheet metal forming
>>analysis. The material can be represented with nonlinear stress-strain properties
>>so that plastic deformation occurs and the metal permanently deforms.
>>
>>The datasheet you cited is the main documentation we have for this solver.
>>If you
>>need more information, I suggest you contact your sales representative and
>>they
>>can hook you up to a local support person.
>>
>>Regards
>>Mark
>>
>>
>>
>>
>>
>>
>>"Li Pingshan" wrote:
>>>
>>>Hi,
>>>
>>>I saw UGS website (http://www.ugs.com/products/nx/docs/fs_nastran_nonlinear.pdf)
>>>shown a sheet metal foeming analysis. I hope to know,
>>>
>>>1.Whether this is a permanent deformation or a 'large deformation' which

>>will
>>>be
>>>
>>>fully reversed back after load released?
>>>2.Is Nastran able to perform such sheet metal forming (permanent) analysis?
>>>Where
>>>
>>>can I get such related information?
>>>
>>>Thanks in advanced.
>>>
>>>Best Rgds
>>>Pingshan

>>
>