Cancel
Showing results for 
Search instead for 
Did you mean: 

Shock response spectrum analysis

Creator
Creator
Dear Nastran/FEMAP users,
I have to perform a SRS analysis, applying a SRS load as follows to an assembly model:

500 Hz -> 500 g
3000 Hz -> 2000 g
10000 Hz -> 2000 g

I have never done that: how do I apply this load to my model? Is there any tutorial or example available?

Thanks

Marco
1 REPLY

Re: Shock response spectrum analysis

N/A

Marco,
There is a section in the NXN Advanced Dynamics guide that discusses shock response
simulation. It covers both creation of a spectrum from a transient solution and
the use of the spectrum. I think you are interested in the use of the spectrum so
concentrate on that part.
I have attached an example model you can review.
Mark




dtmtech wrote:
>
>Dear Nastran/FEMAP users,
>I have to perform a SRS analysis, applying a SRS load as follows to an
>assembly model:
>
>500 Hz -> 500 g
>3000 Hz -> 2000 g
>10000 Hz -> 2000 g
>
>I have never done that: how do I apply this load to my model? Is there
>any tutorial or example available?
>
>Thanks
>
>Marco
>
>
>--
>dtmtech
>------------------------------------------------------------------------
>dtmtech's Profile: http://bbsnotes.ugs.com/vbulletin/member.php?userid=198072
>View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=40225
>