cancel
Showing results for 
Search instead for 
Did you mean: 

Solver 106 vs. 601,106

Pioneer
Pioneer

Good Afternoon Guys,

 

Can anyone explain to me what are the main differences between Solver 106 and Solver 601,106? Also when is best to use one instead of the other?

 

Thanks in advance,

Loismen

3 REPLIES

Re: Solver 106 vs. 601,106

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Loismen,

Well, nothing to see, SOL601 is really powerful and the price is rather competitive, SOL106 is quite limited in many aspects, specially in contact: surface-to-surface contact is not supported, only 1-D CGAP node-to-node and Slide-Line contact elements are supported. Also the limitation in Large Strain < 10% is really a handicap, but I use SOL106 a lot as well, is very easy to setup any nonlinear analysis and when the nonlinear problem involve contact or more complex aspect then I move to Advanced Nonlinear SOL601.

nonlinear-basic-vs-advanced.png

 

nonlinear-contact-elements-nxnastran-sol106.png

Please note SIEMENS is working since years in a native nonlinear code named SOL401 that will have soon the best of both worlds!!.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Solver 106 vs. 601,106

Pioneer
Pioneer
Thank you for your answer. It was really helpful. Regards, Loismen

Re: Solver 106 vs. 601,106

Legend
Legend

SOL106 is the legacy NL solver, dating from before MSC acquired Marc.  SOL601,106 is an integration of NX NASTRAN and Adina (very much the same way MSC has done with Marc) and offers a much greater amount of non-linear ability (contact, post-buckling, element birth/death,...), to bring it on par with the other big two non-linear solvers on the market.  SOL106 is decently capable for mildly non-linear problems, but really can't compare to SOL601,106...  106 comes bundled with the basic NX NASTRAN module, but 601 is an add-on...