Cancel
Showing results for 
Search instead for 
Did you mean: 

Spring type!'?

Experimenter
Experimenter

Hello.

Wich is the different between Celas translational and rotational?

 

What is the meaning of component end A and B when you select the type.?

2 REPLIES

Re: Spring type!'?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Hoyos,

Take a look to the NX NASTRAN ELEMENT LIBRARY user manual, there you have all the information required to understand and know the nastran resources used by NX AdvSim.

 

CELASxx is a Scalar spring element that connect two degrees of freedom at two different grid point. They behave like simple extension/compression or rotational (e.g. clock) springs, carrying either force or moment loads. Forces result in translational (axial) displacement and moments result in rotational displacement. CELAS1 and CELAS2 are the only two types supported in NX AdvSim. You can define translational stiffness as well as rotational stiffness. EndA and EndB are the both ends of the element, each node in the case of a two-nodes CELAS2 element.

 

scalar-elements.png

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Spring type!'?

Siemens Phenom Siemens Phenom
Siemens Phenom

In addition to the CELAS elements, NX Nastran also includes the CBUSH element. The CBUSH is more convenient because it is capable of defining stiffness in all 6 degrees of freedom, whereas the CELAS elements allow you to define stiffness in only 1 degree of freedom per node that the element connects. A single CBUSH can accomplish the work of 6 CELAS elements. NX Advanced Simulation supports CELAS and CBUSH elements.

 

Regards,

Mark

 

Mark Lamping

Simulation Product Management

Product Engineering Software

 

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

mark.lamping@siemens.com

www.siemens.com/plm