Cancel
Showing results for 
Search instead for 
Did you mean: 

*UGRENT* SOL 103 Displaying More Modes

Experimenter
Experimenter

I'm fairly new to NX 11 and NX simcenter.  I'm trying to run a random vibrations simulation using the response dynamics option (SOL 103) and see the results of everything up to 5000Hz; however, when I run the simulation, it only shows the first 10 modes which only corressponds to up to 1500Hz.  How do I set up my solver so that it will display the necessary number of modes so that I can get up to the necessary frequencies?

 

Thanks.

1 REPLY

Re: *UGRENT* SOL 103 Displaying More Modes

Phenom
Phenom

check what you set up on you EIGR(L) card - 10 is usally a default value

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)