Cancel
Showing results for 
Search instead for 
Did you mean: 

User information message 7555 (etetgd)

N/A
Hallo,

I have made an analysis with "NX Nastran Design- Solver". After performing the analysis the following error occurs in *.f06- file:

*** USER INFORMATION MESSAGE 7555 (ETETGD)
FINITE ELEMENT GEOMETRY CHECK RESULTS EXCEED TOLERANCE LEVELS FOR THE FOLLOWING ELEMENTS.
USER ACTION: USE THE GEOMCHECK (EXECUTIVE CONTROL STATEMENT) KEYWORD=VALUE TO CHANGE TOLERANCE VALUES IF DESIRED.
ALL EDGE LENGTH TO HEIGHT RATIO (AR)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY FAIL.
A MINIMUM OF 100 EDGE NODE POINT LENGTH RATIO (ER)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY xxxx.
EDGE ANGLE VALUES ARE INDICATED BY AN * AFTER THE VALUE. THE TOLERANCE LIMIT IS 30 DEGREES.
ALL NEG/ZERO DET(JACOBIAN) VALUE (DJ)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY FAIL.
A MINIMUM OF 100 NEG DET(JAC) AT VERTEX NODE (DG)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY xxxx.
1 SOLUTION 1 JUNE 23, 2010 NX NASTRAN 9/17/09 PAGE 9

There are no results in simulation navigator.
What do I need to change, that the simulation can be solved?
To change tolerance values in EXECUTIVE CONTROL STATEMENT as suggested in the error description, is not possible in NX Nastran Design solver, right? How can I change it with this solver? Or do I need NX Nastran Desktop Solver?

Thanks for your help,

Sarah
3 REPLIES

Re: User information message 7555 (etetgd)

N/A
Dear Sarah,
The message you send do not include the full report of the error, if the cause of the error is due for a very bad mesh quality in the *.F06 you will see written the element(s) number and the cause of the error (Aspect Ratio, etc..), but your message is incomplete, I do not see any element number. With NX Nastran if an element violates the minimun quality required simple the solver stop solution. In fact, you can include nx nastran keywords in the solution in order to avoid (to increase) the mesh quality check, but it is not recomended at all. Simply RE-MESH your model reducing your global element size and you will see that the mesh quality will increase, then NX NASTRAN solver will accept the model for solving.
Revise your geometry, simplify the geometry deleting (or supressing) very small details that will cause the mesher to create degenerated elements or highly distorted mesh, OK?
Best regards,
Blas.
--
~~~~~~~~~~~~~~~~~~~~~~
Blas Molero Hidalgo
Ingeniero Industrial
Director

IBERISA
Edificio Ercilla
Rodríguez Arias 23, 3º - Dpto. 19
48011 BILBAO (SPAIN)
Tel. (+34) 94 410 65 50
Fax. (+34) 94 470 26 34
E-mail: info@iberisa.com
WEB: http://www.iberisa.com
"SarahS" escribió en el mensaje de noticias newsSmiley FrustratedarahS.4d06sz@noreply.bbsnotes.ugs.com...
>
> Hallo,
>
> I have made an analysis with "NX Nastran Design- Solver". After
> performing the analysis the following error occurs in *.f06- file:
>
> *** USER INFORMATION MESSAGE 7555 (ETETGD)
> FINITE ELEMENT GEOMETRY CHECK RESULTS EXCEED TOLERANCE LEVELS FOR
> THE FOLLOWING ELEMENTS.
> USER ACTION: USE THE GEOMCHECK (EXECUTIVE CONTROL STATEMENT)
> KEYWORD=VALUE TO CHANGE TOLERANCE VALUES IF DESIRED.
> ALL EDGE LENGTH TO HEIGHT RATIO (AR)TOLERANCE LIMIT VIOLATIONS
> WILL BE IDENTIFIED AND INDICATED BY FAIL.
> A MINIMUM OF 100 EDGE NODE POINT LENGTH RATIO (ER)TOLERANCE
> LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY xxxx.
> EDGE ANGLE VALUES ARE INDICATED BY AN *
> AFTER THE VALUE. THE TOLERANCE LIMIT IS 30 DEGREES.
> ALL NEG/ZERO DET(JACOBIAN) VALUE (DJ)TOLERANCE LIMIT VIOLATIONS
> WILL BE IDENTIFIED AND INDICATED BY FAIL.
> A MINIMUM OF 100 NEG DET(JAC) AT VERTEX NODE (DG)TOLERANCE
> LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY xxxx.
> 1 SOLUTION 1
> JUNE 23, 2010 NX NASTRAN 9/17/09 PAGE 9
>
> There are no results in simulation navigator.
> What do I need to change, that the simulation can be solved?
> To change tolerance values in EXECUTIVE CONTROL STATEMENT as suggested
> in the error description, is not possible in NX Nastran Design solver,
> right? How can I change it with this solver? Or do I need NX Nastran
> Desktop Solver?
>
> Thanks for your help,
>
> Sarah
>
>
> --
> SarahS
> ------------------------------------------------------------------------
> SarahS's Profile: http://bbsnotes.ugs.com/vbulletin/member.php?userid=192703
> View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=42643
>

Re: User information message 7555 (etetgd)

N/A
Hi Blas,

thanks for your information. Here is the rest of the *.f06 file.

*** USER INFORMATION MESSAGE 7555 (ETETGD)
FINITE ELEMENT GEOMETRY CHECK RESULTS EXCEED TOLERANCE LEVELS FOR THE FOLLOWING ELEMENTS.
USER ACTION: USE THE GEOMCHECK (EXECUTIVE CONTROL STATEMENT) KEYWORD=VALUE TO CHANGE TOLERANCE VALUES IF DESIRED.
ALL EDGE LENGTH TO HEIGHT RATIO (AR)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY FAIL.
A MINIMUM OF 100 EDGE NODE POINT LENGTH RATIO (ER)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY xxxx.
EDGE ANGLE VALUES ARE INDICATED BY AN * AFTER THE VALUE. THE TOLERANCE LIMIT IS 30 DEGREES.
ALL NEG/ZERO DET(JACOBIAN) VALUE (DJ)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY FAIL.
A MINIMUM OF 100 NEG DET(JAC) AT VERTEX NODE (DG)TOLERANCE LIMIT VIOLATIONS WILL BE IDENTIFIED AND INDICATED BY xxxx.
1 SOLUTION 1 JUNE 23, 2010 NX NASTRAN 9/17/09 PAGE 9

0
TOLERANCE LIMITS ARE: TET_AR = 100.00, TET_EPLR = 0.50, TET_DETJ = 0.00, TET_DETG = 0.00 (xxxx = LIMIT VIOLATED)
LONGEST SHORTEST ASPECT EDGE POINT MIN. JACOBIAN MIN. DET(JAC)
ELEMENT TYPE ID EDGE HEIGHT RATIO LENGTH RATIO DETERMINANT AT VERTEX
TETRA 666 1.43 0.89 1.61 0.86*xxxx 1.49 1.36
TETRA 1171 1.64 0.73 2.24 0.86*xxxx 1.50 1.38
TETRA 2336 1.10 0.38 2.89 0.86*xxxx 0.37 0.31
TETRA 2685 1.08 0.46 2.34 0.68*xxxx 0.19 0.10
TETRA 3383 1.95 0.71 2.75 0.86*xxxx 1.61 1.50
TETRA 3384 1.95 0.85 2.29 0.86*xxxx 1.74 1.59
TETRA 4055 1.01 0.36 2.77 0.67*xxxx 0.08 0.00
TETRA 5000 1.79 0.69 2.62 0.69*xxxx 1.39 1.31
TETRA 5263 1.42 0.88 1.62 0.82*xxxx 1.38 1.23
TETRA 5917 1.98 0.85 2.33 0.84*xxxx 2.37 2.15
TETRA 5921 1.98 0.73 2.72 0.84*xxxx 1.48 1.31
TETRA 7803 1.40 0.90 1.55 0.86*xxxx 1.48 1.35
TETRA 7821 1.34 0.88 1.52 0.84*xxxx 1.19 1.06
TETRA 8030 1.76 0.71 2.48 0.86*xxxx 1.52 1.40
TETRA 8104 1.88 0.78 2.41 0.82*xxxx 1.59 1.47
TETRA 8135 2.00 0.81 2.47 0.82*xxxx 2.03 1.72
TETRA 9320 1.98 0.80 2.47 0.80*xxxx 1.63 1.45
TETRA 9984 1.70 0.93 1.84 0.80*xxxx 2.17 1.90
TETRA 10057 1.51 0.66 2.28 0.84*xxxx 0.83 0.72
TETRA 10158 1.28 0.65 1.96 0.86*xxxx 0.83 0.76
TETRA 10172 1.51 0.50 3.00 0.69*xxxx 0.58 0.45
TETRA 10378 1.62 0.72 2.25 0.85*xxxx 1.59 1.40
TETRA 11634 0.80 0.34 2.32 0.67*xxxx 0.07 0.00
TETRA 11812 1.63 0.51 3.22 0.86*xxxx 0.80 0.65
TETRA 11961 1.10 0.49 2.24 0.69*xxxx 0.22 0.15
TETRA 12169 1.48 0.88 1.67 0.86*xxxx 1.31 1.20
TETRA 12528 1.75 0.56 3.11 0.86*xxxx 1.03 0.83
TETRA 12989 1.52 0.87 1.75 0.80*xxxx 1.59 1.28
TETRA 13068 1.08 0.37 2.90 0.68*xxxx 0.23 0.18
TETRA 13404 1.43 0.52 2.75 0.68*xxxx 0.72 0.53
TETRA 13406 1.43 0.23 6.32 0.68*xxxx 0.22 0.17
TETRA 13448 1.04 0.61 1.71 0.86*xxxx 0.57 0.51
TETRA 13551 1.52 0.84 1.81 0.80*xxxx 1.50 1.27
TETRA 13563 1.52 0.79 1.92 0.82*xxxx 1.47 1.20
TETRA 13677 1.76 0.88 1.99 0.83*xxxx 2.34 2.12
TETRA 13716 1.66 0.65 2.54 0.80*xxxx 0.96 0.83
TETRA 13819 1.71 0.81 2.12 0.83*xxxx 1.84 1.65
TETRA 13822 1.78 0.81 2.18 0.83*xxxx 2.06 1.86
TETRA 14025 1.27 0.25 5.19 0.93 0.12 -0.01 xxxx
TETRA 14164 1.88 0.76 2.48 0.82*xxxx 1.76 1.53
TETRA 14180 1.72 0.81 2.12 0.86*xxxx 1.87 1.71
TETRA 14203 1.55 0.56 2.79 0.80*xxxx 0.87 0.68
1 SOLUTION 1 JUNE 23, 2010 NX NASTRAN 9/17/09 PAGE 10


I try your suggestion with the mesh.

Thanks,

Sarah

Re: User information message 7555 (etetgd)

N/A
Hallo Blas,

I have changed the mesh type and decreased the element size. Now it works.

Thank you very much,

Sarah