Showing results for 
Search instead for 
Do you mean 
Reply

What means F06 Warnings

Hello Experts,

what do the following F06 File warnings mean:

>>>>>>>>>>>>>>>

*** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE   4334 BEAM     ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.
 *** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE    147 BUSH     ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.
 *** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE    822 HEXA     ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.
 *** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE     30 PENTA    ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.
 *** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE    467 PYRAM    ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.
 *** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE  47944 QUAD8    ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.
 *** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE  92236 TETRA    ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.
 *** USER INFORMATION MESSAGE 4507 (SDREE)
     IN SUBCASE         1                    
     THERE ARE   5780 TRIA6    ELEMENTS HAVING STRAIN ENERGY WHICH IS LESS THAN   0.0010 PERCENT
     OF THE TOTAL STRAIN ENERGY OF ALL ELEMENTS.

<<<<<<<<<<<<<<<

 

My model consists of a lot different element types and I have to manipulate a lot of PARAMETERS to get it solvable:

AutoMPC = YES,
MaxRatio = 1e11,
PRGPST = NO.

Does it mean that I have no appropriate load in my solution or did I "wring" my model with my PARAMETERS in a unusual way?

 

Any suggestion can help, with best regards, Michael.

 

 

2 REPLIES

Re: What means F06 Warnings

The messages mean exatly what they say. At the end of the analysis, there are elements which have very low strain energies. This means that they have no load going through them. They are either in an unloaded area of the structure, or they could not be connected to the rest of the structure.

 

Note that these are "User Information Messages", not Warnings, Errors or Fatals.

Re: What means F06 Warnings

JimB,

 

thank you for your answer.

As beeing only a user information message I think I do not need it, because I ckeck my model using other ways.

 

That's why is here my last question in this topic: Can I switch it off?

 

Michael