Cancel
Showing results for 
Search instead for 
Did you mean: 

Which is better between SOL 106 or SOL 601/106 for post-buckling analysis?

Creator
Creator

Hi,

 

I am planning to do a nonlinear static post-buckling analysis. The only nonlinearity are the geometric ones, the material is considered linear elastic. Which module of Nx Nastran I should use? SOL 106 or 601,106

I have done some tests and they gave me different results for certain cases. Which one I should trust?

 

Thank you 

1 REPLY

Re: Which is better between SOL 106 or SOL 601/106 for post-buckling analysis?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Enric,

Both solvers are capable to solve nonlinear buckling problems with success, large strain > 10% is a clear limitation of SOL106, but geometric-only nonlinear post-buckling analysis using Basic NonLinear NX NASTRAN (SOL106) could be performed using Arc-Length Control (Riks Method) perfectly.

nonlinear-basic-vs-advanced.pngBest regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/