Cancel
Showing results for 
Search instead for 
Did you mean: 

import mesh into Geometry in UG

N/A

Hi There,
Is there any way to inport a mesh (exported into nastran input deck file)into the
geometry where originately it has been created.
The issue is i need to export my mesh to be able to create my laminate in another
package and bring my mesh back into UGI.
after this operation, i loose the geometry so i cant have an iterative process.
is there any possible way, might be with an API programm to be able to import a
mesh and stick it in the geometry where originally has been created?
Best regards,
3 REPLIES

Re: import mesh into Geometry in UG

Pioneer
Pioneer
Importing the mesh back into FEMAP, you can use the Modifiy->Associativity command to reconnect the mesh to the geomety.
Hope this helps,
Carlton.

Re: import mesh into Geometry in UG

N/A

Thanks Carlton, but i am using NX6 not FEMAP.
Regards,

carlton wrote:
>
>Importing the mesh back into FEMAP, you can use the
>Modifiy->Associativity command to reconnect the mesh to the geomety.
>Hope this helps,
>Carlton.
>
>
>--
>carlton
>------------------------------------------------------------------------
>carlton's Profile: http://bbsnotes.ugs.com/vbulletin/member.php?userid=192482
>View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=38047
>

Re: import mesh into Geometry in UG

N/A
Hello!,
Till I know not remedy exist, in NX6 AdvSim not possible to re-associate mesh with geometry, but you can do it in FEMAP v10.1, a command exist to automatically associate nodes & elements with geometry, then this can be done perfectly in NX6 AdvSim if developers receive input from users requesting this feature to implemented in NX AdvSim, I am with you and this feature is welcome to be in NX AdvSim, please put pressure to developers.
Best regards,
Blas.
--
~~~~~~~~~~~~~~~~~~~~~~
Blas Molero Hidalgo
Ingeniero Industrial
Director

IBERISA
Edificio Ercilla
Rodríguez Arias 23, 3º - Dpto. 19
48011 BILBAO (SPAIN)
Tel. (+34) 94 410 65 50
Fax. (+34) 94 470 26 34
E-mail: info@iberisa.com
WEB: http://www.iberisa.com
"engrequest" escribió en el mensaje de noticias news:4ad2ed42$1@bbsnotes.ugs.com...
>
> Hi There,
>
> Is there any way to inport a mesh (exported into nastran input deck file)into the
> geometry where originately it has been created.
> The issue is i need to export my mesh to be able to create my laminate in another
> package and bring my mesh back into UGI.
> after this operation, i loose the geometry so i cant have an iterative process.
> is there any possible way, might be with an API programm to be able to import a
> mesh and stick it in the geometry where originally has been created?
>
> Best regards,