Cancel
Showing results for 
Search instead for 
Did you mean: 

negative tangent modulus in TableS1 (sol601)

N/A

Hi,
i am performing an advanced non linear analysis using contact. i am considering
small strain and displacement so i am using the true engineering strain Vs stress
data.
but it does issue an error when reading nastran data complaining that the tangent
modulus is negative in TableS1 for the material.
could you please shed any light on this?
Many thanks,
Engrequest


7 REPLIES

Re: negative tangent modulus in TableS1 (sol601)

N/A

"engrequest" wrote:
>
>Hi,
>
>i am performing an advanced non linear analysis using contact. i am considering
>small strain and displacement so i am using the true engineering strain Vs
>stress
>data.
>but it does issue an error when reading nastran data complaining that the
>tangent
>modulus is negative in TableS1 for the material.
>could you please shed any light on this?
>
>Many thanks,
>Engrequest
>
>
>
>

Hi,
probably you filled the table with some wrong values. TABLES1 uses linear estrapolation
outside the table, maybe it is the extrapolation. Could you post the TABLES1 from
your bulk (bdf or dat) file?
Anyway if you consider small displacement and small strain (hence the only non linearity
is the contact) you should not need any TABLES1.
Hope this helps
Francesco

Re: negative tangent modulus in TableS1 (sol601)

N/A

"francesco pelizza" wrote:
>
>"engrequest" wrote:
>>
>>Hi,
>>
>>i am performing an advanced non linear analysis using contact. i am considering
>>small strain and displacement so i am using the true engineering strain Vs
>>stress
>>data.
>>but it does issue an error when reading nastran data complaining that the
>>tangent
>>modulus is negative in TableS1 for the material.
>>could you please shed any light on this?
>>
>>Many thanks,
>>Engrequest
>>

>
>Hi,
>probably you filled the table with some wrong values. TABLES1 uses linear
>estrapolation
>outside the table, maybe it is the extrapolation. Could you post the TABLES1
>from
>your bulk (bdf or dat) file?
>Anyway if you consider small displacement and small strain (hence the only
>non linearity
>is the contact) you should not need any TABLES1.
>
>Hope this helps
>Francesco
The error message simply means that one (or more) of the segments of your stress-strain
curve has a negative slope. As noted by remark 9 for MATS1 in the QRG:
If TYPE = ¡°PLASTIC¡±, all tangent modulii ETi must satisfy the following:
HR = 1: 0 ¡Ü ETi < E
HR = 2: 0.0001 * E < ETi < E
HR = 3: 0.0001 * E < ET < E
Note that in the upcoming NX Nastran 7 release, this restriction will be removed
and a negative slope will be allowed, if that is what you truly need.
Also note that this is not an extrapolation issue. Linear extrapolation simply extends
the last segment as needed. If the last segment has positive slope, so will the
extrapolated data.
Regards,
Jim

Re: negative tangent modulus in TableS1 (sol601)

N/A

"Jim Bernard" wrote:
>
>"francesco pelizza" wrote:
>>
>>"engrequest" wrote:
>>>
>>>Hi,
>>>
>>>i am performing an advanced non linear analysis using contact. i am considering
>>>small strain and displacement so i am using the true engineering strain

>Vs
>>>stress
>>>data.
>>>but it does issue an error when reading nastran data complaining that the
>>>tangent
>>>modulus is negative in TableS1 for the material.
>>>could you please shed any light on this?
>>>
>>>Many thanks,
>>>Engrequest
>>>

>>
>>Hi,
>>probably you filled the table with some wrong values. TABLES1 uses linear
>>estrapolation
>>outside the table, maybe it is the extrapolation. Could you post the TABLES1
>>from
>>your bulk (bdf or dat) file?
>>Anyway if you consider small displacement and small strain (hence the only
>>non linearity
>>is the contact) you should not need any TABLES1.
>>
>>Hope this helps
>>Francesco
>
>The error message simply means that one (or more) of the segments of your
>stress-strain
>curve has a negative slope. As noted by remark 9 for MATS1 in the QRG:
>
> If TYPE = ¡°PLASTIC¡±, all tangent modulii ETi must satisfy the following:
>
>
> HR = 1: 0 ¡Ü ETi < E
> HR = 2: 0.0001 * E < ETi < E
> HR = 3: 0.0001 * E < ET < E
>
>Note that in the upcoming NX Nastran 7 release, this restriction will be removed
>and a negative slope will be allowed, if that is what you truly need.
>
>Also note that this is not an extrapolation issue. Linear extrapolation simply
>extends
>the last segment as needed. If the last segment has positive slope, so will
>the
>extrapolated data.
>
>Regards,
>Jim
Dear all,
of course the error message means that there is a negative slope on the stress strain
curve (it is in the question Engrequest posted). I still think that if Engrequest
would post the TABLES1 we could help him better than reporting the QRG, I also think,
as stated in the preceding post, that if he wants to perform an analysis with small
strains and displacements in which the non linearity is only the contacts the real
problem is that he should not use MATS1 (and corresponding TABLES1) that are used
for material non linearity.
I'm happy than in the NX Nastran 7 release this limitation there is not anymore
(as it is already in MSC NASTRAN), but I really don't think it is what Engrequest
need, or meant with this post.
Regards
Francesco

Re: negative tangent modulus in TableS1 (sol601)

N/A

"francesco pelizza" wrote:
>
>Dear all,
>of course the error message means that there is a negative slope on the stress
>strain
>curve (it is in the question Engrequest posted). I still think that if Engrequest
>would post the TABLES1 we could help him better than reporting the QRG, I
>also think,
>as stated in the preceding post, that if he wants to perform an analysis with
>small
>strains and displacements in which the non linearity is only the contacts
>the real
>problem is that he should not use MATS1 (and corresponding TABLES1) that are
>used
>for material non linearity.
>
>I'm happy than in the NX Nastran 7 release this limitation there is not anymore
>(as it is already in MSC NASTRAN), but I really don't think it is what Engrequest
>need, or meant with this post.
>
>Regards
>Francesco
>
>

Actually, if the model is truly linear in all respects except for contact, he could
use SOL 101 (which MSC does not have) rather than SOL 601.

Re: negative tangent modulus in TableS1 (sol601)

N/A

Dear All,
Iam applying the Sol601 for the contact surfaces and as well to consider the non
linearity of the material ( ( when perfoming a sol101 i had a lof of stress on the
contact surfaces (high compressive load applied) )
when i tried the basic non linear, the contact surfaces were not modelled proferly
with gap elements so the soltuino was not converging so i decided to go for the
sol601.
i used the same stress strain curve i have used for sol106 but for the sol601 i
had the error or negative tangent modulus.

> francesco, this is the TableS1 on the bulk data &colon;

$* NX Material: HIGH-STRENGTH_STEEL
MAT1 11.8600+8 0.3100008.0000-6 25.0000
MATS1 1 1 PLASTIC 1 11.5500+6
TABLES1 1 +
+ 0.0000 0.00000.0083331.5500+60.010000 1600.000.020000 1700.00+
+ 0.040000 1800.000.050000 1900.00 ENDT
$*
Thanks,

"francesco pelizza" wrote:
>
>"Jim Bernard" wrote:
>>
>>"francesco pelizza" wrote:
>>>
>>>"engrequest" wrote:
>>>>
>>>>Hi,
>>>>
>>>>i am performing an advanced non linear analysis using contact. i am considering
>>>>small strain and displacement so i am using the true engineering strain

>>Vs
>>>>stress
>>>>data.
>>>>but it does issue an error when reading nastran data complaining that the
>>>>tangent
>>>>modulus is negative in TableS1 for the material.
>>>>could you please shed any light on this?
>>>>
>>>>Many thanks,
>>>>Engrequest
>>>>
>>>
>>>Hi,
>>>probably you filled the table with some wrong values. TABLES1 uses linear
>>>estrapolation
>>>outside the table, maybe it is the extrapolation. Could you post the TABLES1
>>>from
>>>your bulk (bdf or dat) file?
>>>Anyway if you consider small displacement and small strain (hence the only
>>>non linearity
>>>is the contact) you should not need any TABLES1.
>>>
>>>Hope this helps
>>>Francesco

>>
>>The error message simply means that one (or more) of the segments of your
>>stress-strain
>>curve has a negative slope. As noted by remark 9 for MATS1 in the QRG:
>>
>> If TYPE = ¡°PLASTIC¡±, all tangent modulii ETi must satisfy the following:
>>
>>
>> HR = 1: 0 ¡Ü ETi < E
>> HR = 2: 0.0001 * E < ETi < E
>> HR = 3: 0.0001 * E < ET < E
>>
>>Note that in the upcoming NX Nastran 7 release, this restriction will be
>removed
>>and a negative slope will be allowed, if that is what you truly need.
>>
>>Also note that this is not an extrapolation issue. Linear extrapolation simply
>>extends
>>the last segment as needed. If the last segment has positive slope, so will
>>the
>>extrapolated data.
>>
>>Regards,
>>Jim

>
>Dear all,
>of course the error message means that there is a negative slope on the stress
>strain
>curve (it is in the question Engrequest posted). I still think that if Engrequest
>would post the TABLES1 we could help him better than reporting the QRG, I
>also think,
>as stated in the preceding post, that if he wants to perform an analysis with
>small
>strains and displacements in which the non linearity is only the contacts
>the real
>problem is that he should not use MATS1 (and corresponding TABLES1) that are
>used
>for material non linearity.
>
>I'm happy than in the NX Nastran 7 release this limitation there is not anymore
>(as it is already in MSC NASTRAN), but I really don't think it is what Engrequest
>need, or meant with this post.
>
>Regards
>Francesco
>
>

Re: negative tangent modulus in TableS1 (sol601)

N/A

"engrequest" wrote:
>
>Dear All,
>
>Iam applying the Sol601 for the contact surfaces and as well to consider the
>non
>linearity of the material ( ( when perfoming a sol101 i had a lof of stress
>on the
>contact surfaces (high compressive load applied) )
>when i tried the basic non linear, the contact surfaces were not modelled
>proferly
>with gap elements so the soltuino was not converging so i decided to go for
>the
>sol601.
>i used the same stress strain curve i have used for sol106 but for the sol601
>i
>had the error or negative tangent modulus.
>
>> francesco, this is the TableS1 on the bulk data &colon;

>$* NX Material: HIGH-STRENGTH_STEEL
>MAT1 11.8600+8 0.3100008.0000-6 25.0000
>MATS1 1 1 PLASTIC 1 11.5500+6
>TABLES1 1 +
>+ 0.0000 0.00000.0083331.5500+60.010000 1600.000.020000 1700.00+
>+ 0.040000 1800.000.050000 1900.00 ENDT
>$*
>Thanks,
>
With that data, the second segment of the stress-strain curve has a negative modulus:
Strain Stress Slope
-------- -------- ------------
0 0
0.008333 1.55E+06 186007440.3
0.01 1600 -928854229.2
0.02 1700 10000
0.04 1800 5000
0.05 1900 10000

If you plot this data, the chart certainly does not look correct. Are you sure that
the last 4 stress values are not off by a factor of 1000? The following data would
be valid and "looks" more like a typical stress-strain curve:
Strain Stress Slope
-------- -------- ------------
0 0
0.008333 1.55E+06 186007440.3
0.01 1600000 29994001.2
0.02 1700000 10000000
0.04 1800000 5000000
0.05 1900000 10000000
Regards,
Jim

Re: negative tangent modulus in TableS1 (sol601)

N/A

Thanks Jim,
normally i write the stress strain cruve data on the NX interface in the material
properties (values are in N)
it seems that in writing the imput solver file, there is an issue with the units,
because the first value of stress (yield ) is written in mN and the next ones in
N that's why i am having a factor of 1000 missing.
Regards,
"Jim Bernard" wrote:
>
>"engrequest" wrote:
>>
>>Dear All,
>>
>>Iam applying the Sol601 for the contact surfaces and as well to consider

>the
>>non
>>linearity of the material ( ( when perfoming a sol101 i had a lof of stress
>>on the
>>contact surfaces (high compressive load applied) )
>>when i tried the basic non linear, the contact surfaces were not modelled
>>proferly
>>with gap elements so the soltuino was not converging so i decided to go for
>>the
>>sol601.
>>i used the same stress strain curve i have used for sol106 but for the sol601
>>i
>>had the error or negative tangent modulus.
>>
>>> francesco, this is the TableS1 on the bulk data &colon;

>>$* NX Material: HIGH-STRENGTH_STEEL
>>MAT1 11.8600+8 0.3100008.0000-6 25.0000
>>MATS1 1 1 PLASTIC 1 11.5500+6
>>TABLES1 1 +
>>+ 0.0000 0.00000.0083331.5500+60.010000 1600.000.020000 1700.00+
>>+ 0.040000 1800.000.050000 1900.00 ENDT
>>$*
>>Thanks,
>>
>
>With that data, the second segment of the stress-strain curve has a negative
>modulus:
>
> Strain Stress Slope
> -------- -------- ------------
> 0 0
> 0.008333 1.55E+06 186007440.3
> 0.01 1600 -928854229.2
> 0.02 1700 10000
> 0.04 1800 5000
> 0.05 1900 10000
>
>
>If you plot this data, the chart certainly does not look correct. Are you
>sure that
>the last 4 stress values are not off by a factor of 1000? The following data
>would
>be valid and "looks" more like a typical stress-strain curve:
>
> Strain Stress Slope
> -------- -------- ------------
> 0 0
> 0.008333 1.55E+06 186007440.3
> 0.01 1600000 29994001.2
> 0.02 1700000 10000000
> 0.04 1800000 5000000
> 0.05 1900000 10000000
>
>Regards,
>Jim