Cancel
Showing results for 
Search instead for 
Did you mean: 

printing node in natural sorted way - save eigenvectors using output4

Experimenter
Experimenter

Does a command / setting exist suchs that the nodes are printed on the input deck in a natural sorting order? Thus 1,2,3,4,5,.... etc. 

 

Further is it possible to store the eigenvectors using the output4 format after a SOL103 run?

 

Best regards

Karim

2 REPLIES

Re: printing node in natural sorted way - save eigenvectors using output4

Creator
Creator
I believe I can answer the first question. The nodes should be exported in numeric order if you uncheck the performance export option under Advanced Solver Options.

Re: printing node in natural sorted way - save eigenvectors using output4

Experimenter
Experimenter

Yes this worked, thanks!

 

Further does anyone has an idea concerning the storage of eigenvectors? If i'm not mistaking the output4 format was developd specifically to store matrices, as such cant the eigenvectors be stored as a [Num_nodes x 6] matrix?