Cancel
Showing results for 
Search instead for 
Did you mean: 

"Invalid Deck" error

Innovator
Innovator
NX Nastran 6.0

We have an issue that has GTAC baffled. I thought someone else may have run into this.

We have a user that wants to be able to run simulations from home. All of Nastran is installed on his laptop. His solve files are also local. He attaches to a VPN account in order to pull a license. A solve will work fine when connected to the network will solve fine. However, when connecto to the VPN, he gets the following error:

------------
16:02:57 NX NASTRAN Authorization Information - Checkout Successful
16:02:57 ----------------------------------------------------------
16:02:57 License for module NX Nastran Basic - NX Desktop checked out successfully


16:02:58 NX NASTRAN Authorization Information - Invalid Deck
16:02:58 ---------------------------------------------------
16:02:58 The BULK DATA section has been either hand
16:02:58 edited, or the deck was generated on
16:02:58 another machine

-----------


We have checked the following:
HOSTNAME is not changing
checked composite id with/without vpntext compare of the .dat and .log files match, other than trivial date/time
tested in-house with/without dock to eliminate dock

Any other ideas?
TCUA 8.3.3
NX 7.5.2
SE ST3 MP 11
2 REPLIES

Re: "Invalid Deck" error

Siemens Builder Siemens Builder
Siemens Builder
1) Export the deck while connected to the network at work
2) Export the deck while connected via VPN at home

Are the checksums written to the ENDDATA card for the two decks the same?
--
Jim Bernard
Advanced Applications Engineer

Siemens PLM Software
2000 Eastman Dr., Milford, OH 45150-2712
www.siemens.com/plm

Re: "Invalid Deck" error

Innovator
Innovator
Forgot to put that in. already c hecked and the checksums are the same.

1) Export the deck while connected to the network at work
2) Export the deck while connected via VPN at home

Are the checksums written to the ENDDATA card for the two decks the same?
TCUA 8.3.3
NX 7.5.2
SE ST3 MP 11