Cancel
Showing results for 
Search instead for 
Did you mean: 

"No Results are Found" - Problem with imported Nastran solver deck to solve modal analysis case

Hi

 

I prepared a modal analysis(geometry, mesh, materials, etc..) in Hypermesh and then generated a Nastran solver deck, a .bdf file, to import no Siemens NX 10 and solve it with Nastran Solver. (Case 1)

I also did the same analysis, from the beggining, in Siemens NX 10 and solved it (SOL 103 - Real Eigenvalues) with success. (Case 2)

 

Happens that when i import the .bdf file and then run the solver, goes everything ok but then i can't see the results, "No Results are Found".

I already checked both .f06 files, from Case 1 and 2 and i can see that in Case 1, Nastran was able to find solutions, wich match the ones from Case 2.

I also tried with bailout to -1 but goes the same way.

Any sugestion?

 

Thank you

 

Miguel Duarte

2 REPLIES

Re: "No Results are Found" - Problem with imported Nastran solver deck to solve modal **bleep**

Siemens Phenom Siemens Phenom
Siemens Phenom

Does the input deck contain output requests (i.e. DISP(PLOT) = ALL)?

Is PARAM, POST, -2 specified?

 

Can you post the .f06 and .log files from the run?''

 

Can you post the NX syslog?

Re: "No Results are Found" - Problem with imported Nastran solver deck to solve modal **bl

Hey

 

I didn't had any of those parameters defined but i already tried with them on and it worked.

Thank you very much!