Cancel
Showing results for 
Search instead for 
Did you mean: 

traction pressure

Experimenter
Experimenter

i have a cantilever plate. one end of the plate is fixed and the other end has a follower traction pressure applied of 100 MPa. how do you apply follower traction in NX /? is it right to use sol 601 for this analysis ? if possible, please put screenshots. thank you.

1 REPLY

Re: traction pressure

Siemens Phenom Siemens Phenom
Siemens Phenom

If the plate is modeled with solid elements, then you can define a pressure load (PLOAD4) to get the desired behavior. Pressures are follower loads (normal to the element face) when they aren't given a direction.

 

If the plate is modeled as shell elements, then you have no option but to use a FORCE entry in NASTRAN. NASTRAN doesn't support edge based pressures. NX 9 added follower force support by supporting the NASTRAN FORCE1 and FORCE2 entries. 

 

1. Select the Force command

2. Set the Type to Magnitude and Direction

3. Set the Direction Method to Along 2 Nodes or Normal to 4 Nodes

 

Those methods in step 3 create FORCE1 and FORCE2 entries. In NASTRAN, as the nodes move, the force directions update.

 

Regards,

Mark

 

Mark Lamping

Simulation Product Management

Product Engineering Software

 

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

mark.lamping@siemens.com