Showing results for 
Search instead for 
Do you mean 
Reply

uniaxial cyclic plasticity...

Hi,

Can anyone tell how should I be able to apply a alternating displacement on one face of a cube. The variation of displacement is from 0.025 to -0.025 with time.

 

 

Thanks

2 REPLIES

Re: uniaxial cyclic plasticity...

Assuming you are running Advanced Nonlinear (SOL 601,106), you create a time varying displacement load using DLOAD/TLOAD/TABLED and SPCD.

 

DLOAD        301     1.0     1.0      10
TLOAD1        10      11               1      12
TABLED1       12                                                        +
+            0.0     0.0     1.0     1.0     2.0    -1.0     3.0     1.0+
+            4.0    -1.0     5.0     0.0    ENDT
SPCD          11   10001       1     1.0

 

 

 

Re: uniaxial cyclic plasticity...

Is this possible in NX9?