cancel
Showing results for 
Search instead for 
Did you mean: 

Academic 2D flow simulation

Experimenter
Experimenter

Hello,

 

This is my first post. I am investigating NX11 and I'd like to make a very simple case to introduce CFD theory and NX tool to master students at University through some practical lessons.

 

The idea is to make a pure 2D flow simulation so that students can compare the results with analytical solutions. The case is a 2D wing section.

 

Is there such a possibility in NX11? I searched for it but I coundn't find anything.

 

Regards,

Dimitri

 

 

2 REPLIES

Re: Academic 2D flow simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, this can be done with NX Flow.

 

Start with the online documentation here: https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:xid1128419:index_advanced:id1245911

Re: Academic 2D flow simulation

Experimenter
Experimenter

Thanks JimB.

I searched the online documentation but I found nowhere that case of pure 2D simulation.

 

What I did is in short

- a sketch

- extrude

- mesh 2D dependent on top and bottom face (Reference CSYS : cartesian / absolute)

- 3D swept mesh from bottom face with element size the same as my extrude length, meaning I have ony one cell on the z axis

- Within the simulation frame, I selected "Simulation object type -> Symmetry plan" on the upper surface, then repeat for lower face.

You can have a look in the screenshot attached.

pure2Dflow.png

The result is a pure 2D flow, the w velocity is null everywhere.

 

Nevertheless, I think the computation is performed with two times the number of dof that it should.

 

Here are the info for my 2D mesh:

MESH INFORMATION
Name : 2d_mesh(1)
Type of mesh : 2D
Export Mesh to Solver : True
Number of elements in the mesh : 7427
Number of nodes in the mesh : 3869
Tri3 Thin Shell elements : 7427
Layer : 1

MESH COLLECTOR INFORMATION
Name : Shell(1)
Type : Shell

MESH RECIPE INFORMATION
Element Type : TRI3 Thin Shell

 

 

And here are the info for my 3D mesh:

MESH INFORMATION
Name : 3d_mesh(1)
Type of mesh : 3D
Number of elements in the mesh : 7427
Number of nodes in the mesh : 7738
Wedge6 elements : 7427
Layer : 1

MESH COLLECTOR INFORMATION
Name : Solid(2)
Type : Solid

==== Material
Type : Pure Substance
Material : Air


MESH RECIPE INFORMATION
Element Type : HEXA8

 

How can I impose that the solution on the upper side shall be the same as the one on the lower side ?

Using automatic coupling? or Mapping Constraints? or Periodic boundary Conditions (I don't find it in NX11)?

 

Thanks for the help,

Dimitri