Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

Air flow in an electronic box with NX thermal/Flow

[ Edited ]

Hello

 

I am doing a Coupled flow and thermal analysis for an electronic box and using NX Thermal/Flow 10.

And use the fan which is volume  rate of 70CFM.

Heat load is 100 Watt and atmosphere temperature is 50 degC.

Box material and other materials are aluminium 6061.

 

After steady state analysis, the maximum fluid temperature is 50 degC.

Whereas initial condition the fluid temperature was 50 degC.

and I did not see warming any surface neither heat source nor any surface.

 

Can somebody help me this problem?

5 REPLIES

Re: Air flow in an electronic box with NX thermal/Flow

Hi CastawaY,

 

check if in "solve options" you choose both : solve thermal, solve flow

check also your heat load if it is defined properly

 

Best,

Sami

Re: Air flow in an electronic box with NX thermal/Flow

Hi Sami

 

solve thermal and flow has been chosen. You can see  attachment.

heat load is correct.

 

I solved this design another cae program. There was no problem.

I don't understand what is wrong.

 

Best,

Oz

Solution
Solution
Accepted by topic author CastawaY
‎05-09-2016 09:27 AM

Re: Air flow in an electronic box with NX thermal/Flow

Hi OZ,

 

Have you tried to use flow/thermal coupled solver? not NX Electronic System Cooling.

and don't forget to define coupling between disconnected geometries (for thermal)

 

Best,

Sami

Re: Air flow in an electronic box with NX thermal/Flow

Is anything defined as a flow surface?  If not, there won't be any convection...

Re: Air flow in an electronic box with NX thermal/Flow

Hi Sami

 

Thanks alot.

I solved the problem with your help.