Cancel
Showing results for 
Search instead for 
Did you mean: 

Can NX Nastran Thermal Solution model phase change?

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

From the documentation it seems:

 

1) I can enter material properties for phase change

 

2) I can inspect the phase change as a result of a NX thermal/flow solution

 

Can NX nastran thermal model phase change? I can specify the material property in the material library. But I am not sure if NX nastran thermal is actually using those properties for the calcution.

 

Thanks!

2 REPLIES

Re: Can NX Nastran Thermal Solution model phase change?

Community Manager Community Manager
Community Manager

@Carl_P think you can answer this one?


Regards,
Ganesh

Simcenter 3D Community Manager
Simulation and Test Solutions

Re: Can NX Nastran Thermal Solution model phase change?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

According to the NXN9 QRG the MAT4 card does include phase change temperature and latent heat of fusion.  You would need to run SOL159 for time-dependency, and all the usual considerations for running non-linear would apply.