Cancel
Showing results for 
Search instead for 
Did you mean: 

Change axis resolution in FEM analysis

Experimenter
Experimenter

Hi

I made a FEM simulation of a wave washer. To set some constraints I made some small auxiliary structures. Now I have the problem that stresses at the constraints are much higher than in the rest of the part. Has anybody an idea how one can zoom in that it is possible to see also low stresses? And how can i check strains/stresses in a single element? I am using NX 9.

Thanks for your help.

1 REPLY
Highlighted

Re: Change axis resolution in FEM analysis

Siemens Phenom Siemens Phenom
Siemens Phenom

This is done on the Legend tab of the Post View dialog.

 

Pick Edit Post View EditPostView.png

 

On the Legend tab, Set Color and Value Control to Specified and enter the desired Min/Max values. You can also adjust the number of bands, etc.

 

PostViewDialog.png