Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

Change axis resolution in FEM analysis

Hi

I made a FEM simulation of a wave washer. To set some constraints I made some small auxiliary structures. Now I have the problem that stresses at the constraints are much higher than in the rest of the part. Has anybody an idea how one can zoom in that it is possible to see also low stresses? And how can i check strains/stresses in a single element? I am using NX 9.

Thanks for your help.

1 REPLY
Solution
Solution
Accepted by topic author srk
‎07-22-2016 10:43 AM

Re: Change axis resolution in FEM analysis

This is done on the Legend tab of the Post View dialog.

 

Pick Edit Post View EditPostView.png

 

On the Legend tab, Set Color and Value Control to Specified and enter the desired Min/Max values. You can also adjust the number of bands, etc.

 

PostViewDialog.png