Cancel
Showing results for 
Search instead for 
Did you mean: 

Cleaning up NX Flow image

N/A

NX6
I did a sample file, which consists of a wing element, an end plate, and a pylon,
plus a large box of "air" around it all. Now I'm looking at the results, and there
is a lot of info away from the wing, that I'd like to not see...I'd like to see
just the pressures, and velocities on the wing/endplate/pylon surfaces.
I used the Fluid Domain method to mesh the block of air, with a plane of symmetry
on the centerline face, the bottom is a smooth surface, and all other sides are
open. I let the solver find the wing/endplate/pylon on it's own, rather than specifically
pick them as Flow Blockage.
Is is it possible to get data displayed for just the wing surfaces? I've been hunting
thru the Docs, and CAST, but have not found it yet. I've also been trying to get
"streamlines", and have not muddled thru that to get those yet either.
Dave Kieffer
www.rileytech.com
Riley Technologies LLC
170 Overhill Drive
Mooresville, NC 28117
5 REPLIES

Re: Cleaning up NX Flow image

N/A

"Dave Kieffer" wrote:
>
>
>
>NX6
>
>I did a sample file, which consists of a wing element, an end plate, and a
>pylon,
>plus a large box of "air" around it all. Now I'm looking at the results,
>and there
>is a lot of info away from the wing, that I'd like to not see...I'd like to
>see
>just the pressures, and velocities on the wing/endplate/pylon surfaces.
>
>I used the Fluid Domain method to mesh the block of air, with a plane of symmetry
>on the centerline face, the bottom is a smooth surface, and all other sides
>are
>open. I let the solver find the wing/endplate/pylon on it's own, rather than
>specifically
>pick them as Flow Blockage.
>
>Is is it possible to get data displayed for just the wing surfaces? I've
>been hunting
>thru the Docs, and CAST, but have not found it yet. I've also been trying
>to get
>"streamlines", and have not muddled thru that to get those yet either.

Dave,
Velocities are (by definition) zero at the surface, so you won't be able to display
these without the fluid elements.
You can request Surface Pressure output on the Edit Solution, Results Options tab
under 3D Flow. This will generate surface pressure results on the non fluid elements.
To create streamlines, generate a post display of velocity, fluid pressure, etc.
with the fluid elements displayed. Then right click on the Viewports, Fringe Plots,
Post View item on the Post Processing Navigator and select Create Streamlines. Create
a seed set, then OK out of all of the forms to get the streamline display.

Re: Cleaning up NX Flow image

N/A

"Jim Bernard" wrote:
>
>"Dave Kieffer" wrote:
>>
>>
>>
>>NX6
>>
>>I did a sample file, which consists of a wing element, an end plate, and

>a
>>pylon,
>>plus a large box of "air" around it all. Now I'm looking at the results,
>>and there
>>is a lot of info away from the wing, that I'd like to not see...I'd like

>to
>>see
>>just the pressures, and velocities on the wing/endplate/pylon surfaces.
>>
>>I used the Fluid Domain method to mesh the block of air, with a plane of

>symmetry
>>on the centerline face, the bottom is a smooth surface, and all other sides
>>are
>>open. I let the solver find the wing/endplate/pylon on it's own, rather

>than
>>specifically
>>pick them as Flow Blockage.
>>
>>Is is it possible to get data displayed for just the wing surfaces? I've
>>been hunting
>>thru the Docs, and CAST, but have not found it yet. I've also been trying
>>to get
>>"streamlines", and have not muddled thru that to get those yet either.

>
>Dave,
>
>Velocities are (by definition) zero at the surface, so you won't be able to
>display
>these without the fluid elements.
>
>You can request Surface Pressure output on the Edit Solution, Results Options
>tab
>under 3D Flow. This will generate surface pressure results on the non fluid
>elements.
>
>To create streamlines, generate a post display of velocity, fluid pressure,
>etc.
>with the fluid elements displayed. Then right click on the Viewports, Fringe
>Plots,
>Post View item on the Post Processing Navigator and select Create Streamlines.
>Create
>a seed set, then OK out of all of the forms to get the streamline display.
Thanks, that helps a lot!! It would still be nice if you could turn off the elements
on the fluid, so you can see the results better. Also, if you could make the results
translucent, so you could get a better 3D image of whats going on, when in the shaded/banded
type views.
-Dave
-Dave
Dave Kieffer
www.rileytech.com
Riley Technologies LLC
170 Overhill Drive
Mooresville, NC 28117

Re: Cleaning up NX Flow image

N/A

"Dave Kieffer" wrote:
>
>Thanks, that helps a lot!! It would still be nice if you could turn off the
>elements
>on the fluid, so you can see the results better. Also, if you could make
>the results
>translucent, so you could get a better 3D image of whats going on, when in
>the shaded/banded
>type views.
>
>-Dave
>
>-Dave
>Dave Kieffer
>www.rileytech.com
>Riley Technologies LLC
>170 Overhill Drive
>Mooresville, NC 28117
>

Dave,
You can make the results translucent.
First, you will have to turn on global translucency support.
- Pick Preferences, Visualization
- On the Visual tab, toggle on Translucency
Now, to make the results translucent, pick Post View (the camera icon)
- On the Edges & Faces tab, set the primary display faces to translucent
You may also want to experiment with the cutting plane. This is on the Post View
display tab. Set Display On to Cutting Plane and use the Options button to define/move
the plane.
Regards,
Jim

Re: Cleaning up NX Flow image

N/A

"Jim Bernard" wrote:
>
>"Dave Kieffer" wrote:
>>
>>Thanks, that helps a lot!! It would still be nice if you could turn off

>the
>>elements
>>on the fluid, so you can see the results better. Also, if you could make
>>the results
>>translucent, so you could get a better 3D image of whats going on, when in
>>the shaded/banded
>>type views.
>>
>>-Dave
>>
>>-Dave
>>Dave Kieffer
>>www.rileytech.com
>>Riley Technologies LLC
>>170 Overhill Drive
>>Mooresville, NC 28117
>>

>
>Dave,
>
>You can make the results translucent.
>
>First, you will have to turn on global translucency support.
> - Pick Preferences, Visualization
> - On the Visual tab, toggle on Translucency
>
>Now, to make the results translucent, pick Post View (the camera icon)
> - On the Edges & Faces tab, set the primary display faces to translucent
>
>You may also want to experiment with the cutting plane. This is on the Post
>View
>display tab. Set Display On to Cutting Plane and use the Options button to
>define/move
>the plane.
>
>Regards,
>Jim
>
Jim,
Thanks again, I'll give this a try...you've been much more helpful than the docs.
-Dave
Dave Kieffer
www.rileytech.com
Riley Technologies LLC
170 Overhill Drive
Mooresville, NC 28117

Re: Cleaning up NX Flow image

N/A

"Jim Bernard" wrote:
>
>"Dave Kieffer" wrote:
>>
>>Thanks, that helps a lot!! It would still be nice if you could turn off

>the
>>elements
>>on the fluid, so you can see the results better. Also, if you could make
>>the results
>>translucent, so you could get a better 3D image of whats going on, when in
>>the shaded/banded
>>type views.
>>
>>-Dave
>>
>>-Dave
>>Dave Kieffer
>>www.rileytech.com
>>Riley Technologies LLC
>>170 Overhill Drive
>>Mooresville, NC 28117
>>

>
>Dave,
>
>You can make the results translucent.
>
>First, you will have to turn on global translucency support.
> - Pick Preferences, Visualization
> - On the Visual tab, toggle on Translucency
>
>Now, to make the results translucent, pick Post View (the camera icon)
> - On the Edges & Faces tab, set the primary display faces to translucent
>
>You may also want to experiment with the cutting plane. This is on the Post
>View
>display tab. Set Display On to Cutting Plane and use the Options button to
>define/move
>the plane.
>
>Regards,
>Jim
>
Jim,
Thanks again, I'll give this a try...you've been much more helpful than the docs.
-Dave
Dave Kieffer
www.rileytech.com
Riley Technologies LLC
170 Overhill Drive
Mooresville, NC 28117