Cancel
Showing results for 
Search instead for 
Did you mean: 

Cloning FEM-model

Creator
Creator

Hi,

to simulate several variants of a model, I create renamed sim-files with the command "Create Clone Assembly". This copies and renames all files that are connected to the Sim file.

When opening the cloned Sim file, however, all links between the files (SIM, AFM, FEM, PRT) are lost and have to be redifined.

Can this be avoided?

 

Greetings

Werner

1 REPLY

Re: Cloning FEM-model

Siemens Phenom Siemens Phenom
Siemens Phenom

You can do a "Save As" in the highest level part that you want to duplicate. For example, a save as in the SIM will only "copy" the SIM. A save as in the FEM will prompt for a new FEM and SIM file name, etc.