Cancel
Showing results for 
Search instead for 
Did you mean: 

Comparing mode shapes of 2 FEMs - Creating a MAC calc in NX.CAE?

Phenom
Phenom

To all

 

Is there a way of doing  a MAC calc (Modal Assurance Criterion) with the mode shapes of 2 FEMs.

I have a highly refined FEM of a part and a simplifed one. I am looking for a way of comparing the mode shapes (maybe using a MAC calc: scalar constant relating the degree of consistency (linearity) between one modal and another reference modal vector) rather than relying on the "it looks similar"

 

With the modal vectors (mode shape) available is there a way in NX.CAE to do such MAC calc?

 

Thanks

Regards

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)
1 REPLY

Re: Comparing mode shapes of 2 FEMs - Creating a MAC calc in NX.CAE?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

This can be done with NX FE Model Correlation, which is an add-on to NX Advanced FEM. You can also do side-by-side animations of modes that are paired by the MAC.

 

Phil

 

 


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com