Cancel
Showing results for 
Search instead for 
Did you mean: 

Conversion of the results to the local material coordinate system

Hi everyone,


NX 9.0.2.5

 

I met some problem, as I understand (if not, please correct me) all the results by default are displayed for the SOL101 for the global coordinate system, however I need to display them with respect to the local material coorinate system for the shell elements. How shall I do this ?

 

Thanks for help Smiley Happy

3 REPLIES

Re: Conversion of the results to the local material coordinate system

Hi, I can see that nobody replied.

 

... I have found such tip in Siemens Documentation (see screenshot)

Can anyone tell me how to transform the results and / or display the CSYS that is currently used for the result duisplay ? When I load my results there is no current CSYS in the Simulation Navigator.

 

Thanks for help.

Re: Conversion of the results to the local material coordinate system

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Tomek,

 

Which result are you interested in? Not all results types can be transformed. If you edit your post view, click on results beside color display:

 

14-Jul-15 7-31-09 AM.png

 

You can see which systems are available for the currently posted result.

 

The Selected option works if the coordinate system in question is included in your fem and is part of the solution. For that, you need to go back to the fem, create the csys and refer to it - for example, as a nodal displacement coordinate system.

 

Phil


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com

Re: Conversion of the results to the local material coordinate system

Thanks Phil,

 

That's what I wanted ! Smiley Happy