Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

Create Group of Nodes Associated with Mesh Point

Hello,

Is there a way to create a group containing just the nodes associate with mesh points?

Thanks

John

2 REPLIES

Re: Create Group of Nodes Associated with Mesh Point

Hi John,

First define a group of all your mesh points by setting the type filter to mesh point. Then create a second group and set the method to related nodes and select as input the group of mesh points. As a result you should get a group of nodes that are related to the mesh points.

Regards,

xtof

 

Solution
Solution
Accepted by Ganesh_S (Community Manager)
‎08-26-2015 04:32 AM

Re: Create Group of Nodes Associated with Mesh Point

Note that the intermediate group containing mesh points is not required. When the New Group dialog is open, set the Smart Selection Method (red outline in the image below) to "Related Nodes", then pick the mesh points.

 

Also note: if other visible entities (i.e. polygon faces or meshes) are taking precedence in the selector, you can also set the selection Type filter (yellow outline) to Mesh Points.

 

 

 

Regards,

Jim